This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137: Problem with ECC, vFill vs Fill

Part Number: TMS570LS3137
Other Parts Discussed in Thread: NOWECC, UNIFLASH,

Hello,

During the implementation of the CRC calculation of the whole flash content (safety mechanism required by the TMS570 safety manual), we got some uncorrectable ECC error that we traced back to unused flash locations. Our linker script includes the following:

MEMORY
{
    VECTORS (X)  		: origin=0x00000000 length=0x00000060
    KERN_FUNC (RX)		: origin=0x00000060 length=0x0000FF0F vfill = 0xffffffff
	FLASH0  (RX)		: origin=0x00010000 length=0x002F0000 vfill = 0xffffffff

After compilation generates the following .map file:

MEMORY CONFIGURATION

         name            origin    length      used     unused   attr    fill
----------------------  --------  ---------  --------  --------  ----  --------
  VECTORS               00000000   00000060  00000020  00000040     X
  KERN_FUNC             00000060   0000ff0f  00008494  00007a7b  R  X
  FLASH0                00010000   002f0000  002f0000  00000000  R  X  ffffffff 

For instance, only 0x8494 bytes out of 0xFF0F are used in the KERN_FUNC section. We get the ECC error at 0xC000, which is in the used part. According to the linker documentation, the vfill specifier is sufficient to force ECC generation for the whole section and not just the parts that are filled. But when generating the ECC with nowECC we see the following:

PS C:\...\build> .\nowECC.exe -i .\input.hex -f021 16M_ADD -a -o .\output.hex
This is nowECC Version 2.22
Mapping: F021-16MB

ECC calculation from 0x00000000 to 0x0000001F
ECC calculation from 0x00000060 to 0x000084F7
ECC calculation from 0x00010000 to 0x00058ABF
*** Appending ECC section to file -> .\output.hex
No Errors

So the ECC is generated only until address 0x84F7.

Then if we change the vfill specifier to just fill in the linker script, the ECC gets generated for the whole flash (as expected), ECC error does not appear, BUT the size of the binary naturally also drastically increases.

Is there some particularity of the vfill specifier that I am missing?

Thank you for your help,

Aaron