This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Expert,
The customer tries to use MSP-GANG to burn the image to MSPM0L1105 of the customized board, but "ERROR 23" will be displayed.
I changed ports 1, 3, and 4 of MSP-GANG but the same error message appears.
Customers can program successfully using XDS110
flash tool Pin define refer to the picture below.
The question looks similar to the discussion below
Do you have any normal use cases or related information?
How to solve the problems that customers are encountering now?
Thanks
Daniel
Hi Daniel,
Refer below thread, make sure the connection of the MSP-GANG is correct (sometimes, I find user will mistake the PIN 1 of the interface).
B.R.
Sal
Hi Sal
The customer has confirmed that the signal wiring is correct.
Is there anything else that needs to be confirmed?
Thanks
Daniel
Hi Daniel,
Please make sure customer connect the PIN2 (rather than PIN4) to the MCU VCC if they choose the programmer power supply.
The question looks similar to the discussion below
B.R.
Sal