Part Number: LP-AM243
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hello;
I have been working with single chip servo example for AM243-Lp board. (/ti/motor_control_sdk_am243x_09_02_00_09/examples/tidep_01032_dual_motor_drive/single_chip_servo/am243x-lp/).
I integrated the single chip servo project into my own project and I am rotating two motors at a fixed speed on the r5 1-0 core. I am running the ethercat slave application on the r5 0-0 core. When I debug the project via CCS, the motors are rotating and the software is running. However, when I flash this software to the device memory with uniflash, the motors draw more current and do not rotate. What could be the reason that could create this effect between the debug process and flashing the software?
Regards
Kadir