This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCU-PLUS-SDK-AM263X: How to use MCAN3 on AM263x-LaunchPad?

Part Number: MCU-PLUS-SDK-AM263X
Other Parts Discussed in Thread: AM2634, LP-AM263

Tool/software:

Hello,

for my application I want to use three MCAN modules.

The LaunchPad provides MCAN0 directly and MCAN1 by external pin mux on J7.63 and J7.64.

Furthermore the AM263x LaunchPad User Guide shows in table 4-25 "Pinmux Options for J7" that "MCAN3_RX" and "MCAN3_TX" can be made available on J7.69 and J7.70 in Mode0.

At the same time it claims that in Mode0 "ADC3_AIN2" and "DAC_OUT" (showing in green) are the Default signals J7.69 and J7.70. I assume something got twisted in this table because the pink Muxed alternative signals are shown in the Mode8 column and not as expected in the Mode0 column.

I refer to SPRUJ10D – MAY 2022 – REVISED SEPTEMBER 2023.

What ModeX and external pin mux do I have to chose to get access to MCAN1 and MCAN3 on J7 header or anywhere else on the LaunchPad?

Thanky you.

Antonius

  • Antonius,

    MCAN1 can be accessed on J7-63 and J7-64. The MuxMode=0. In order to have MCAN1 on these BoosterPack pins, the SEL signal on the upstream MUX U52 needs to be configured HIGH in order for the path A<->C to be enabled.

    MCAN3 can be accessed on J7-69 and J7-70. The MuxMode=0 for MCAN3_RX (AM2634 pin C14) and the MuxMode=0 for MCAN3_TX (AM2634 pin A15). The same MUX U52 needs to be configured with the SEL signal HIGH in order to enable the correct path.

    Please refer to the LP-AM263 design files for the full on-board MUX routing, as well as the source pin for the MUX U52 SEL signal: https://www.ti.com/lit/zip/sprr452  

    Regards,

    Brennan