This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello.
I opened sysconfig to change pin settings in a project I was using. However, it showed the following message and could not be opened.
Please let me know what the problem is.
So I loaded the example project of MCU-PLUS-SDK-AM263X for testing. I still can't open sysconfig in the example project.
Thank you.
Hi Jae,
Apologies you had to face this issue. Could you help em with following:
Which SDK version are you using and which syscfg version are you using?
Hello
Thank you for your answer.
I tried several things before checking your answer.
And fortunately, I solved it, although I don't know the cause.
option : Window - Preferences -> General - Appearence -> Enable therming[ ]
I was using the theme of CCS in dark mode, but due to personal visual problems, I disabled the option to use the theme. When I did that, the problem occurred.
option : Window - Preferences -> General - Appearence -> Enable therming[V]
When I re-enabled the option to use the theme, I was able to load sysconfig normally.
The SDK is version 9.1.0.41, and sysconfig is using version 1.19.0.
And the CCS version is using version 12.6.0.00008.
If there are no additional problems, I will use it as is.
Thank you.