This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/EK-TM4C1294XL: LaunchPad SPI coumnication with 7x10 R click

Part Number: EK-TM4C1294XL

Tool/software: TI-RTOS

Hi.

I have trouble with Tiva  TM4C1294XL and  SPI interface.

i have to use 7×10 R click – dual character display to display some number in several speeds!

I need some help howe can i write a number or character over SPI ?

every answer is welcome !

Thank you !!!

  • Do you have a specific question about using the TM4C1294? Are you using the EK-TM4C1294XL launchpad for your development? You can see a simple SPI example in TivaWare

    C:\ti\TivaWare_C_Series-2.1.4.178\examples\peripherals\ssi

    If you need to use an RTOS, there is a TI-RTOS example included with the TM4C TIRTOS.

    You need to look at documentation for your display to identify what data to send out the SPI.

  • Hello Bob, 

    first thanks for your help.

    I have to programme a modul named 7x10 R click at the Boosterpack 1 of EK-TM4C1294XL in order to display numbers and char's.

    inow i can initialize the SPI. 

    but i have to iniitlaize not only the Chip 74HC595  but and the Chip CD4017 at the same time !!! and i am not so clearly how i have to programme this array to display any number or to set only one darlington diod !!!

    Below some code of me:

    0184.main.c
    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    15
    16
    17
    18
    19
    20
    21
    22
    23
    24
    25
    26
    27
    28
    29
    30
    31
    32
    33
    34
    35
    36
    37
    38
    39
    40
    41
    42
    43
    44
    45
    46
    47
    48
    49
    50
    51
    52
    53
    54
    55
    56
    57
    58
    59
    60
    61
    62
    63
    64
    65
    66
    67
    #include <stdbool.h>
    #include <stdint.h>
    #include <inc/hw_memmap.h>
    /* XDCtools Header files */
    #include <xdc/std.h>
    #include <xdc/cfg/global.h>
    #include <xdc/runtime/System.h>
    #include <xdc/runtime/Error.h>
    #include <xdc/runtime/Memory.h>
    /* BIOS Header files */
    #include <ti/sysbios/BIOS.h>
    #include <ti/sysbios/knl/Task.h>
    /* Currently unused RTOS headers that are needed
    * for advanced features like IPC. */
    #include <ti/sysbios/knl/Semaphore.h>
    #include <ti/sysbios/knl/Mailbox.h>
    #include <ti/sysbios/knl/Event.h>
    #include <ti/sysbios/hal/Timer.h>
    /* Driverlib headers */
    #include <driverlib/gpio.h>
    /* Board Header files */
    #include <Board.h>
    #include <EK_TM4C1294XL.h>
    /* Application headers */
    #include <Blink_Task.h>
    #include <UART_Task.h>
    #include <TCPEcho_Task.h>
    #include <driverlib/sysctl.h>
    #include <driverlib/pin_map.h>
    #include <driverlib/ssi.h>
    #include "BSPIBus.h"
    uint32_t g_ui32SysClock;
    uint32_t ui32SysClock;
    //uint16_t data;
    uint32_t ui32SysClkFreq;
    uint32_t ui32Index;
    uint32_t ui32Data;
    uint32_t ui32SysClkFreq;
    uint32_t g_ui32SysClock; // system clock in Hz
    uint8_t font[10] = {0x7E, 0x0A, 0xB6, 0x9E, 0xCA, 0xDC, 0xFC, 0x0E, 0xFE, 0xDE}; // 7-Segment font, letters 0 to 9
    //****************************************************************************
    // Configuration of SPI (SSI2, on BoosterPack 2 connector, master mode, 9 Mbps)
    //****************************************************************************
    void InitSpi(void)
    {
    // enable peripherals
    SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI2); // enable SSI2 (for SPI)
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ); // enable port Q for SSI I/O-pins
    // configure pins as SSI2 pins
    GPIOPinConfigure(GPIO_PQ0_SSI3CLK); // Q0 for Clk
    GPIOPinConfigure(GPIO_PQ3_SSI3XDAT1); // Q3 for Master Output Slave Input (MOSI)
    GPIOPinConfigure(GPIO_PQ2_SSI3XDAT0); // Q2 for Master Input Slave Output (MISO)
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

  • Initializing the 7x10 R click display is beyond the scope of what I can help you with. You should contact MikroElektronica for help with their device.

  • Thank you!