This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: SPI slave CS and FIFO preloading

Part Number: TMS320F280049C

Dear Manoj

I have a couple additional questions relating to my last posting, "TMS320F280049C: SPI FIFO interrupt".  As I mentioned before, the slave SPI will return up to 40 bytes of data depending on what the master SPI needs.  If the master SPI needs only 4 bytes, it will enable the CS, generate 16 clocks pulses and disable the CS.  My first question is, what happens to the slave SPI at the time the CS is disabled?  Will the slave SPI reset on its own?  What happens to the slave SPI TX FIFO?  Will it be flushed or will it remain as is?  Second, in preparation to the master SPI asking for the data, how do I preload the slave SPI TX FIFO?  Thank you for your time. 

  • Dennis,

    My first question is, what happens to the slave SPI at the time the CS is disabled?  Will the slave SPI reset on its own?  What happens to the slave SPI TX FIFO?  Will it be flushed or will it remain as is?

    When CS is pulled high from SPI master (controller), SPI(slave) will be put in high-impedance state. It however doesn't reset SPI module nor does it flush the SPI TX FIFO

    Second, in preparation to the master SPI asking for the data, how do I preload the slave SPI TX FIFO?  Thank you for your time. 

    Answer depends upon your system requirement.

    If what SPI slave needs to transmit is independent of what SPI master transmits then you can use TX FIFO interrupt to fill-up TX FIFO and keep it ready.

    If SPI slave needs to transmit depends on what SPI master transmits, then SPI slave cannot preempt and fill the FIFO.

    Regards,

    Manoj

  • Dear Manoj

    Thank you for your quick response.  

    When CS is pulled high from SPI master (controller), SPI(slave) will be put in high-impedance state. It however doesn't reset SPI module nor does it flush the SPI TX FIFO

    Then I must manually reset the slave SPI, flush the slave SPI TX FIFO and fill the slave SPI TX FIFO with new data.  How can I know when the CS has been disabled?  

    Answer depends upon your system requirement.

    If what SPI slave needs to transmit is independent of what SPI master transmits then you can use TX FIFO interrupt to fill-up TX FIFO and keep it ready.

    How do I prefill the slave TX FIFO?  Do I use a SPI put or write function such as "SPI_writeDataNonBlocking(SPIA_BASE, sData[i]);"?  Should it be a blocking or nonblocking function?  

  • Dennis,

    Then I must manually reset the slave SPI, flush the slave SPI TX FIFO and fill the slave SPI TX FIFO with new data.  How can I know when the CS has been disabled?  

    You can check the status of GPIO for CS to determine the status. If CS is activated, you can flush SPI TX FIFO manually and re-fill SPI TX FIFO with new data

    How do I prefill the slave TX FIFO?  Do I use a SPI put or write function such as "SPI_writeDataNonBlocking(SPIA_BASE, sData[i]);"?  Should it be a blocking or nonblocking function?

    You can chose either blocking (or) non blocking  option. Both of them write to SPITXBUF register. Only difference is blocking option doesn't allow you to write if the SPI TX FIFO is full.

    Regards,

    Manoj

  • Dear Manoj

    SPIA is a slave module.  For the moment, I'm not using the FIFO.  In registering my SPI interrupt, "Interrupt_register(INT_SPIA_RX, &spiaRxISR);" the "INT_SPIA_RX" interrupt vector is triggered by what?  Is it the receive buffer receiving a bit or being full.  Is it that the SPIA CS being asserted?  All interrupts are being enabled but I never enter the interrupt.  The CS for the slave, SPIA, is being manually applied by the master SPI from a TIVA launch pad.  I've looked at all four signals with a scope.  The clock, CS and TxData from the master all look as they should.  The RxData from the slave looks good but it's not the data that should be transmitted by the slave.  

  • Dennis,

    When SPI slave receive data it should receive SPI RX interrupt and SPIINT will be set. Please check below table.

    Regards,

    Manoj