Part Number: TMS320F28388D
Other Parts Discussed in Thread: UNIFLASH
CPU does not run after loading an image to C28x device using latest uniflash and performing CPU Reset and run action.
To get CPU to run one of the following had to be done:
1. Power cycle CPU
2. Remove computer USB cable connected to FTDI USB. (This effectively removed power from the Isolated side as it is powered by the computer's USB)
So it seems like the software is still holding onto some reset on the JTAG.
This is an issue as my setup is remote. After programming using Uniflash, the product is bricked waiting for someone to power cycle or pull the USB cable.
I've created a ticket 2 years ago, waiting for a fix. The bug ticket says it's resolved, but it still does not work for me.
https://sir.ext.ti.com/jira/browse/EXT_EP-10393
Any suggestions would be helpful. Thanks.
Using: Windows 11, Uniflash 8.1.1.4146, XDS100v2 USB Debug Probe

Also. Clicking the CPU Reset "Reset Now" button more than once produces an error and does nothing to the CPU.