Part Number: TMDSHVMTRINSPIN
Other Parts Discussed in Thread: C2000WARE
Hi,
I am using kit TMDSHVMTRINSPIN with card TMDSCNCD28069MISO. I walked through the hardware configuration of both the board and card in accordance with the Instaspin motion user guide. That is, I have executed the following checks:

and

I am set up to use a DC power supply (not yet powered on).
I connected up the 15VDC input power, turned on the switch, connected the control card via USB to my PC. I can see "XDS100 Class USB Serial Port" show up in Windows Device Manager. I open the Instaspin Motion GUI and it seems to begin to recognize my motor, but then pops this error:

Trouble Reading Register PC: (Error -1142 @ 0x0)
Device blocked debug access because it is currently executing non-debuggable code.
Choose 'Rude Retry' to disable polite mode and force the operation.
I noticed in other forum posts that one suggestion is that this is related to the JTAG debugger losing control. I ensured M3-J5 is populated. What else can I do to troubleshoot this issue?
Thank you,
Eileen