Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: MOTORWARE
Tool/software: Code Composer Studio
We are using our own Inverter and Sensing circuit to run Bldc motor. Before the motor was running fine but we had some issues with our voltage sensing circuit so we replaced the voltage sensing and with that, we also changed the Gate Driver circuit as we were not confident with the previous gate driving circuit.
Now when I run the lab2c everything runs properly for a couple of seconds. The motor also rotates in open loop which confirms that Gate driver is running properly and the voltage values displayed in the watch window, shows that the voltage is also been sensed properly but after some time, the system resets itself and it presents "Error 1142 @0x0". The screenshots of the error are been uploaded at the end of the post.
According to this post, I have power cycled the board (which is to sit for a couple seconds after turning the device off to make sure the memory in the device is fully cleared before turning it back on) and also tried to change the workspace, but it didn't work.
In this post he was using wrong lab experiments, I think I am using correct ones which are from "boostxldrv8301_revB" the address is (C:\ti\motorware\motorware_1_01_00_18\sw\solutions\instaspin_foc\boards\boostxldrv8301_revB\f28x\f2806xF\projects\ccs\proj_lab02c) but I don't think this is the issue because previously I was running the similar programs and they were running fine.
In this post, the problem was "running DELAY_US(ADC_usDELAY) before memcpy (&RamfuncsRunStart, &RamfuncsLoadStart, (Uint32) &RamfuncsLoadSize) and InitFlash();;" but in my program their are no such functions used.
According to this wiki page, "the running firmware on the device may be preventing the JTAG debugger from properly connecting (if the device has flash memory). In these cases, consult the documentation of your device to find out how to unlock it" but I don't know which document to refer and how to do it.
Please help me out.
The screenshot of the error has been posted below :