This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV830x-HC-C2-KIT

Other Parts Discussed in Thread: CONTROLSUITE, INSTASPIN-BLDC

“DRV830x-HC-C2-KIT”

Control Mode :Allows the selection of four different control modes 

Duty Cycle: The motor is commutated using the sensorless algorithm but is driven in an open-loop duty cycle mode. o

Current: The motor is commutated using the sensorless algorithm while the current (torque) is regulated using a PI controller. (Note: An unloaded motor will rapidly accelerate to a very high speed in this mode.)

Velocity: The motor is commutated using the sensorless algorithm while the motor speed is regulated using a PI controller. The output of the speed controller is a PWM duty cycle. 

Cascade: The motor is commutated using the sensorless algorithm while the motor speed is regulated using a PI controller. The output of the speed controller is a motor current command which is regulated by a lower level current PI controller.

BLDC motor is not running in any of four mode. GUI is successfully communicate with control board show not fault and DC input voltage .

please give the some default  parameter value for this motor Antigravity MN4006 KV380.

Regard 

Nitish Kumar

  • Seems like you want to use the InstaSPIN-BLDC with trapezoidal control algorithm in controlSUITE. You may take a look at the documentation as below. 

    QSG-DRV830x-HC-C2-KIT-GUI.pdf at C:\ti\controlSUITE\development_kits\DRV830x-HC-C2-KIT_v105\~GUI

    InstaSPIN-BLDC Sensorless Control.pdf at C:\ti\controlSUITE\development_kits\DRV830x-HC-C2-KIT_v105\InstaSPIN_BLDC\~Doc