This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069M: XDS100V2 connection was not successful

Part Number: TMS320F28069M

CCS: Version: 12.5.0.00007 

Hardware:lanuchpad28069m+8301

question:The connect test in ccs fails

Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
[Start: Texas Instruments XDS100v2 USB Emulator_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\Admin\AppData\Local\TEXASI~1\CCS\
ccs1250\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100/110/510 class product.
This utility will load the adapter 'jioserdesusb.dll'.
The library build date was 'Sep 6 2023'.
The library build time was '09:57:39'.
The library package version is '9.13.0.00201'.
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

I wish I could get help!