Part Number: LAUNCHXL-F28379D
Hello,
I am a University Professor on Power Electronics, using Simulink - C2000 Microcontroller Blockset to develop control algorithms for power converters. We have been recently working on a modular converter, consisting of several half-bridge modules, each modulated by an ePWM block. The duty cycles for these blocks need to change from 0 to 100% (as well as intermediate values) and vice-versa every few PWM cycles. That is, the duty cycles do not vary smoothly, as in conventional converters. The important point is that these sudden changes need to happen concurrently for all ePWM blocks. We are using a model where all ePWM blocks are in a subsystem triggered by ADC interrupts, and have enabled synchronization of all PWM modules (1-6) based on ePWM1, selecting "Pass through" for the rest of the modules. (Also, the PWM frequency is constant and no phase shift is introduced among the PWMs). Based on this, we expected that each ePWM block would generate pulses with the duty cycle calculated and provided to it at each interrupt. However, it appears that all modules apart from ePWM1 update their duty cycles at different time instants. Reading about this issue, we understand that it relates to the global and one shot load registers.
1. Could you please confirm that this is correct? If not, how can we make all PWM blocks take in the provided duty cycles concurrently?
2. If the solution is indeed through the global and one shot load registers, can you confirm whether these are accessible through Simulink (v. R2023a)? If not, can you advise how custom code can be added to the model to set them properly?
Thank you,
Sincerely,
George Orfanoudakis