Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE
Tool/software:
Hi engineers,
I intend to use the Endat routine in controlSUITE\development_kits\BOOSTXL_POSMGR to implement Endat communication via CLB.
However, I have found that some key functions in the routine are not open. For example, PM_endat22_setupPeriph(void) which contains the CLB initialization and configuration function, as well as the sending and receiving functions, are encapsulated in PM_endat22_lib.lib. During the hardware design, it may not be possible to use SPIB and the corresponding CLB Tile as per the routine, and the implementation of the sending and receiving functions will also need to be adjusted and modified as required.
1.Is it possible to open PM_endat22_lib.lib?
2.There is no.sysyconfig in the software routine. Is there something similar to the following diagram (the design block diagram in the tformat document) that can facilitate a clearer and more intuitive transplantation?

Regards,
Lin Haonan