Part Number: TMS320F280049C
Other Parts Discussed in Thread: C2000WARE, TMDSHVMTRINSPIN
Tool/software:
Hi Team, Greetings!
We are trying to evaluate the BLDC Motor as Generator using custom designed Hardware (3-Phase Inverter as rectifier) with TMS320F280049C DSP.
We have gone through the below tickets and Understood that the FOC Algorithm will supports in Generator mode also.
https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/541403/f28035-based-pmsm-for-bldc-motor-control-motor-as-a-generator
So, we are trying to use "Instaspin FOC" labs code to run the module as 3-phase active rectifier.
The default installation path is: .....ti\c2000\C2000Ware_MotorControl_SDK_4_00_00_00\solutions\tmdshvmtrinspin\f28004x.
Please give your valuble support & clarify the below doubts,
1. If we choose correct path (....\solutions\tmdshvmtrinspin\f28004x), then in which lab we can proceed (Lab1/2/3/4....lab12)?
2. In the above ticket, you all mentioned that "Iq_ref" should be in -ve? then what is the Iq_ref value?
3. Is "Iq_ref" setting sufficient to run the motor as generator? if yes, then PWM error will chnage accordingly right?
Thank you in Advance!
Regards,
Chaithanya N.