Other Parts Discussed in Thread: TMS320F28069
I am using the tms320f28069 and I am trying to use RAM1 to be accessible from CPU and CLA . I read the tread :
//e2e.ti.com/support/microcontrollers/c2000/f/171/p/218230/770892#770892
and I used a global acces to the register MMEMCFG but I still having the same problem : access with CLA but not with CPU.
I included parts of the code if any one can help
Thanks
Hamid
Cla1Regs.MMEMCFG.all = CLA_PROG_ENABLE| CLARAM0_ENABLE|CLARAM1_ENABLE|CLA_RAM1CPUE;
_Cla1Prog_Start = _Cla1funcsRunStart;
-heap 0x200
-stack 0x200
// Define a size for the CLA scratchpad area that will be used
// by the CLA compiler for local symbols and temps
// Also force references to the special symbols that mark the
// scratchpad are.
CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
MEMORY
{
/* Note that the memory allocation below does not create sections as necessary for
the CLA on the F2803x.
*/
PAGE 0:
RAML0 : origin = 0x008000, length = 0x000800 /* on-chip RAM (L0-L1)*/
RAML3 : origin = 0x009000, length = 0x001000 /* data RAM (L3) */
OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */
FLASHH : origin = 0x3D8000, length = 0x004000 /* on-chip FLASH */
FLASHG : origin = 0x3DC000, length = 0x004000 /* on-chip FLASH */
FLASHF : origin = 0x3E0000, length = 0x004000 /* on-chip FLASH */
FLASHE : origin = 0x3E4000, length = 0x004000 /* on-chip FLASH */
FLASHD : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */
FLASHC : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */
FLASHA : origin = 0x3F4000, length = 0x003F80 /* on-chip FLASH */
CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
CSM_PWL : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
FPUTABLES : origin = 0x3FD860, length = 0x0006A0 /* FPU Tables in Boot ROM */
IQTABLES : origin = 0x3FDF00, length = 0x000B50 /* IQ Math Tables in Boot ROM */
IQTABLES2 : origin = 0x3FEA50, length = 0x00008C /* IQ Math Tables in Boot ROM */
IQTABLES3 : origin = 0x3FEADC, length = 0x0000AA /* IQ Math Tables in Boot ROM */
BOOTROM : origin = 0x3FF3B0, length = 0x000C10 /* Boot ROM */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */
PAGE 1 :
BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
dataRAM : origin = 0x008800, length = 0x000400 /* on-chip RAM block L1 */
RAML2 : origin = 0x008C00, length = 0x000400 /* on-chip RAM block L2 */
CLA_CPU_MSGRAM : origin = 0x001480, length = 0x000080 /* CLA-R/W, CPU-R message RAM */
CPU_CLA_MSGRAM : origin = 0x001500, length = 0x000080 /* CPU-R/W, CLA-R message RAM */
}
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHA, PAGE = 0
.pinit : > FLASHA, PAGE = 0
.text : > FLASHA, PAGE = 0
codestart : > BEGIN PAGE = 0
ramfuncs : LOAD = FLASHD,
RUN = RAML0,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
PAGE = 0
Cla1Prog : LOAD = FLASHC, /* Note for running from RAM the load and RUN can be the same */
RUN = RAML3,
LOAD_START(_Cla1funcsLoadStart),
LOAD_SIZE(_Cla1funcsLoadSize),
LOAD_END(_Cla1funcsLoadEnd),
RUN_START(_Cla1funcsRunStart),
PAGE = 0
csmpasswds : > CSM_PWL PAGE = 0
csm_rsvd : > CSM_RSVD PAGE = 0
/* Allocate uninitalized data sections: */
.stack : > RAMM0, PAGE = 1
.ebss : > RAMM1, PAGE = 1
.esysmem : > RAMM1, PAGE = 1
Cla1Data : > dataRAM, PAGE = 1
/* Initalized sections go in Flash */
/* For SDFlash to program these, they must be allocated to page 0 */
.econst : > FLASHA PAGE = 0
.switch : > FLASHA PAGE = 0
/* Allocate IQ math areas: */
IQmath : > FLASHA PAGE = 0 /* Math Code */
IQmathTables : > IQTABLES PAGE = 0, TYPE = NOLOAD /* Math Tables In ROM */
Cla1ToCpuMsgRAM : > CLA_CPU_MSGRAM PAGE = 1
CpuToCla1MsgRAM : > CPU_CLA_MSGRAM PAGE = 1
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS PAGE = 0, TYPE = DSECT
DMARAML5 : > RAML5, PAGE = 1
DMARAML6 : > RAML6, PAGE = 1
DMARAML7 : > RAML7, PAGE = 1
DMARAML8 : > RAML8, PAGE = 1
}
SECTIONS
{
/************* DPLIB Sections C28x ************************/
/* ADCDRV_1ch section */
ADCDRV_1ch_Section : > dataRAM PAGE = 1
/* ADCDRV_4ch section */
ADCDRV_4ch_Section : > dataRAM PAGE = 1
/* CNTL_2P2Z section */
CNTL_2P2Z_Section : > dataRAM PAGE = 1
CNTL_2P2Z_InternalData : > dataRAM PAGE = 1
CNTL_2P2Z_Coef : > dataRAM PAGE = 1
}