This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using the tms320f28069 and I am trying to use RAM1 to be accessible from CPU and CLA . I read the tread :
//e2e.ti.com/support/microcontrollers/c2000/f/171/p/218230/770892#770892
and I used a global acces to the register MMEMCFG but I still having the same problem : access with CLA but not with CPU.
I included parts of the code if any one can help
Thanks
Hamid
Cla1Regs.MMEMCFG.all = CLA_PROG_ENABLE| CLARAM0_ENABLE|CLARAM1_ENABLE|CLA_RAM1CPUE;
_Cla1Prog_Start = _Cla1funcsRunStart;
-heap 0x200
-stack 0x200
// Define a size for the CLA scratchpad area that will be used
// by the CLA compiler for local symbols and temps
// Also force references to the special symbols that mark the
// scratchpad are.
CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
MEMORY
{
/* Note that the memory allocation below does not create sections as necessary for
the CLA on the F2803x.
*/
PAGE 0:
RAML0 : origin = 0x008000, length = 0x000800 /* on-chip RAM (L0-L1)*/
RAML3 : origin = 0x009000, length = 0x001000 /* data RAM (L3) */
OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */
FLASHH : origin = 0x3D8000, length = 0x004000 /* on-chip FLASH */
FLASHG : origin = 0x3DC000, length = 0x004000 /* on-chip FLASH */
FLASHF : origin = 0x3E0000, length = 0x004000 /* on-chip FLASH */
FLASHE : origin = 0x3E4000, length = 0x004000 /* on-chip FLASH */
FLASHD : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */
FLASHC : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */
FLASHA : origin = 0x3F4000, length = 0x003F80 /* on-chip FLASH */
CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
CSM_PWL : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
FPUTABLES : origin = 0x3FD860, length = 0x0006A0 /* FPU Tables in Boot ROM */
IQTABLES : origin = 0x3FDF00, length = 0x000B50 /* IQ Math Tables in Boot ROM */
IQTABLES2 : origin = 0x3FEA50, length = 0x00008C /* IQ Math Tables in Boot ROM */
IQTABLES3 : origin = 0x3FEADC, length = 0x0000AA /* IQ Math Tables in Boot ROM */
BOOTROM : origin = 0x3FF3B0, length = 0x000C10 /* Boot ROM */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */
PAGE 1 :
BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
dataRAM : origin = 0x008800, length = 0x000400 /* on-chip RAM block L1 */
RAML2 : origin = 0x008C00, length = 0x000400 /* on-chip RAM block L2 */
CLA_CPU_MSGRAM : origin = 0x001480, length = 0x000080 /* CLA-R/W, CPU-R message RAM */
CPU_CLA_MSGRAM : origin = 0x001500, length = 0x000080 /* CPU-R/W, CLA-R message RAM */
}
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHA, PAGE = 0
.pinit : > FLASHA, PAGE = 0
.text : > FLASHA, PAGE = 0
codestart : > BEGIN PAGE = 0
ramfuncs : LOAD = FLASHD,
RUN = RAML0,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
PAGE = 0
Cla1Prog : LOAD = FLASHC, /* Note for running from RAM the load and RUN can be the same */
RUN = RAML3,
LOAD_START(_Cla1funcsLoadStart),
LOAD_SIZE(_Cla1funcsLoadSize),
LOAD_END(_Cla1funcsLoadEnd),
RUN_START(_Cla1funcsRunStart),
PAGE = 0
csmpasswds : > CSM_PWL PAGE = 0
csm_rsvd : > CSM_RSVD PAGE = 0
/* Allocate uninitalized data sections: */
.stack : > RAMM0, PAGE = 1
.ebss : > RAMM1, PAGE = 1
.esysmem : > RAMM1, PAGE = 1
Cla1Data : > dataRAM, PAGE = 1
/* Initalized sections go in Flash */
/* For SDFlash to program these, they must be allocated to page 0 */
.econst : > FLASHA PAGE = 0
.switch : > FLASHA PAGE = 0
/* Allocate IQ math areas: */
IQmath : > FLASHA PAGE = 0 /* Math Code */
IQmathTables : > IQTABLES PAGE = 0, TYPE = NOLOAD /* Math Tables In ROM */
Cla1ToCpuMsgRAM : > CLA_CPU_MSGRAM PAGE = 1
CpuToCla1MsgRAM : > CPU_CLA_MSGRAM PAGE = 1
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS PAGE = 0, TYPE = DSECT
DMARAML5 : > RAML5, PAGE = 1
DMARAML6 : > RAML6, PAGE = 1
DMARAML7 : > RAML7, PAGE = 1
DMARAML8 : > RAML8, PAGE = 1
}
SECTIONS
{
/************* DPLIB Sections C28x ************************/
/* ADCDRV_1ch section */
ADCDRV_1ch_Section : > dataRAM PAGE = 1
/* ADCDRV_4ch section */
ADCDRV_4ch_Section : > dataRAM PAGE = 1
/* CNTL_2P2Z section */
CNTL_2P2Z_Section : > dataRAM PAGE = 1
CNTL_2P2Z_InternalData : > dataRAM PAGE = 1
CNTL_2P2Z_Coef : > dataRAM PAGE = 1
}
Hi Hamid,
Did you check the value of "Cla1Regs.MMEMCFG" register in register view of CCS (or in memory watch window)? Just to make correct value is getting written into this register from your code.
Regards,
Vivek Singh
Hi Vivek,
I check the register MMEMCFG :
the RAM1E =1 as expected but RAM1CPUE =0 instead of 1 !!!
is is normal ? I read some where that reading this bit return 0 is that correct ?
any idea ?
Hamid
Hi Hamid,
hamid said:is is normal ? I read some where that reading this bit return 0 is that correct ?
Yes that is correct, bits 8, 9, 10 read 0. You can find the description of the issue, and the workaround, in the errata (SPRZ342).
The workaround in the errata,which is also copied in the TRM, should work - you should be able to access the dataRAM from the CPU side. Based on the combination of macros, you should be writing 0x0231 to MMEMCFG; you can check the disassembly while executing to see if this is the value being written to the regsiter; if not then its possible the #defines might be incorrect.
Hi Vishal,
Thank you for getting back to me.
I checked the #defines is correct and it's working when I set the bit RAM0CPUE = 1 too.
Cla1Regs.MMEMCFG.all = CLA_PROG_ENABLE| CLARAM0_ENABLE|CLARAM1_ENABLE|CLA_RAM0CPUE|CLA_RAM1CPUE;
if I put only RAM1CPUE = 1 the CPU can't access to RAML1.
Cla1Regs.MMEMCFG.all = CLA_PROG_ENABLE| CLARAM0_ENABLE|CLARAM1_ENABLE|CLA_RAM1CPUE;
But its fine for me
Thanks again