This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The reason why I’m writing to you is a problem which we observed when using HRPWM and we are not sure what’s causing this:
In this project we are using the microprocessor TMX320F28377D from Texas Instruments.
The PWM modules are clocked with 100 MHz and the PWMs are running at a frequency of 50 kHz (TBPRD = 1000) in “Up-Down Counter Mode”.
It is necessary to have a high resolution duty cycles of the PWMs.
The actual PWM configuration can be seen in the attached file EPwm1Regs_CMPA_0x03E60000_Export.txt (only EPwm1 is configured).
The actual problem which we observed and where we would need help from TI to understand it and ideally to solve it is the following:
Due to HRPWM support we can precisely set the duty of the PWM cycle from 0 to 99.7999% (EPwm register CMPA= from 0x0 to 0x03E5FF00). However, if CMPA=0x03E60000 (precisely at 99.8%) we get a duty of 50% rather than the desired one.
When increasing the value of the register CMPA to 0x03E60100 (i.e. the next possible duty) then the duty is OK again (approx. 99.8005%).
So, only if the CMPA register is set to 0x03E60000, the problem occurs (we get a duty of 50% rather than the desired one).
At a first glance we think we are facing this problem because the falling edge of the duty is in critical proximity to 3 clocks at the end of the PWM cycle.
Attached are three oscilloscope pictures. Each picture shows the PWM which is created by the equivalent value of the CMPA register.
The attached .pdf file summarizes the three CMPA values.
Short summary of the PWM configuration:
PWM modules are clocked with 100 MHz.
Each PWM has a frequency of 50 kHz.
The PWMs are configured for Up-Down Counter Mode and have a Dead Band of 100 ns on both sides.
TBCTL:
PWM_TBCTL_FREE_SOFT(PWM_TBCTL_FREE_SOFT_STOP_AT_END_CYCLE)
PWM_TBCTL_PHSDIR(PWM_TBCTL_PHSDIR_DOWN)
PWM_TBCTL_CLKDIV(PWM_TBCTL_CLKDIV_DIV1)
PWM_TBCTL_HSPCLKDIV(PWM_TBCTL_HSPCLKDIV_DIV1)
PWM_TBCTL_SWFSYNC(ON)
PWM_TBCTL_SYNCOSEL(PWM_TBCTL_SYNCOSEL_DISABLED)
PWM_TBCTL_PRDLD(PWM_TBCTL_PRDLD_SHADOW)
PWM_TBCTL_PHSEN(OFF)
PWM_TBCTL_CTRMODE(PWM_TBCTL_CTRMODE_UP_DOWN)
AQCTLA:
PWM_AQCTLA_CBD = DISABLED
PWM_AQCTLA_CBU = DISABLED
PWM_AQCTLA_CAD = SET
PWM_AQCTLA_CAU = CLEAR
PWM_AQCTLA_PRD = DISABLED
PWM_AQCTLA_ZRO = SET
The HRPWM registers are configured as follows.
HRPCTL:
PWM_HRPCTL_PWMSYNCSELX(0U)
PWM_HRPCTL_TBPHSHRLOADE(OFF)
PWM_HRPCTL_PWMSYNCSEL(OFF)
PWM_HRPCTL_HRPE(ON)
HRCNFG:
PWM_HRCNFG_HRLOADB(LOAD_ON_ ZERO_PRD)
PWM_HRCNFG_CTLMODEB(SEL_CMPHR_OR_TBPRDHR)
PWM_HRCNFG_EDGEMODEB(BOTH)
PWM_HRCNFG_SWAPAB(PWMA_PWMB_UNCHANGED)
PWM_HRCNFG_AUTOCONV(ENABLE)
PWM_HRCNFG_SELOUTB(EPWMXB_OUT_NORMAL)
PWM_HRCNFG_HRLOAD(LOAD_ON_ZERO_PRD)
PWM_HRCNFG_CTLMODE(SEL_CMPHR_OR_TBPRDHR)
PWM_HRCNFG_EDGEMODE(BOTH)
The MEP_ScaleFactor is calculated once by the SFO() function (after the PWMs are configured and prior to setting TBCLKSYNC to 1).
Many thanks in advance for your support.
Attachments:
Picture1: Oscilloscope screenshot when CMPA=0x03E5FF00
Picture2: Oscilloscope screenshot when CMPA=0x03E60000
Picture3: Oscilloscope screenshot when CMPA=0x03E60100
521177 40 R EPwm1Regs_TBCTL 0x0000000F 0x4032 R EPwm1Regs_TBCTL2 0x0000000F 0x0000 R EPwm1Regs_TBCTR 0x0000000F 0x03A2 R EPwm1Regs_TBSTS 0x0000000F 0x0003 R EPwm1Regs_CMPCTL 0x0000000F 0x0100 R EPwm1Regs_CMPCTL2 0x0000000F 0x0000 R EPwm1Regs_DBCTL 0x0000000F 0x8C0B R EPwm1Regs_DBCTL2 0x0000000F 0x0000 R EPwm1Regs_AQCTL 0x0000000F 0x0000 R EPwm1Regs_AQTSRCSEL 0x0000000F 0x0000 R EPwm1Regs_PCCTL 0x0000000F 0x0300 R EPwm1Regs_HRCNFG 0x0000000F 0x1353 R EPwm1Regs_HRPWR 0x0000000F 0x0028 R EPwm1Regs_HRMSTEP 0x0000000F 0x003F R EPwm1Regs_HRCNFG2 0x0000000F 0x0000 R EPwm1Regs_HRPCTL 0x0000000F 0x0001 R EPwm1Regs_GLDCTL 0x0000000F 0x0000 R EPwm1Regs_GLDCFG 0x0000000F 0x0000 R EPwm1Regs_EPWMXLINK 0x0000000B 0x00000000 R EPwm1Regs_AQCTLA 0x0000000F 0x0092 R EPwm1Regs_AQCTLA2 0x0000000F 0x0000 R EPwm1Regs_AQCTLB 0x0000000F 0x0000 R EPwm1Regs_AQCTLB2 0x0000000F 0x0000 R EPwm1Regs_AQSFRC 0x0000000F 0x0000 R EPwm1Regs_AQCSFRC 0x0000000F 0x0000 R EPwm1Regs_DBREDHR 0x0000000F 0x0000 R EPwm1Regs_DBRED 0x0000000F 0x0014 R EPwm1Regs_DBFEDHR 0x0000000F 0x0000 R EPwm1Regs_DBFED 0x0000000F 0x0014 R EPwm1Regs_TBPHS 0x0000000B 0x00000000 R EPwm1Regs_TBPRDHR 0x0000000F 0x0000 R EPwm1Regs_TBPRD 0x0000000F 0x03E8 R EPwm1Regs_CMPA 0x0000000B 0x03E60000 R EPwm1Regs_CMPB 0x0000000B 0x00000000 R EPwm1Regs_CMPC 0x0000000F 0x0000 R EPwm1Regs_CMPD 0x0000000F 0x0000 R EPwm1Regs_GLDCTL2 0x0000000F 0x0000 R EPwm1Regs_TZSEL 0x0000000F 0x4000 R EPwm1Regs_TZDCSEL 0x0000000F 0x0022 R EPwm1Regs_TZCTL 0x0000000F 0x000A R EPwm1Regs_TZCTL2 0x0000000F 0x0000 R EPwm1Regs_TZCTLDCA 0x0000000F 0x0000 R EPwm1Regs_TZCTLDCB 0x0000000F 0x0000 R EPwm1Regs_TZEINT 0x0000000F 0x0000 R EPwm1Regs_TZFLG 0x0000000F 0x0000 R EPwm1Regs_TZCBCFLG 0x0000000F 0x0000 R EPwm1Regs_TZOSTFLG 0x0000000F 0x0000 R EPwm1Regs_TZCLR 0x0000000F 0x0000 R EPwm1Regs_TZCBCCLR 0x0000000F 0x0000 R EPwm1Regs_TZOSTCLR 0x0000000F 0x0000 R EPwm1Regs_TZFRC 0x0000000F 0x0000 R EPwm1Regs_ETSEL 0x0000000F 0xB000 R EPwm1Regs_ETPS 0x0000000F 0x1001 R EPwm1Regs_ETFLG 0x0000000F 0x0008 R EPwm1Regs_ETCLR 0x0000000F 0x0000 R EPwm1Regs_ETFRC 0x0000000F 0x0000 R EPwm1Regs_ETINTPS 0x0000000F 0x0000 R EPwm1Regs_ETSOCPS 0x0000000F 0x0000 R EPwm1Regs_ETCNTINITCTL 0x0000000F 0x0000 R EPwm1Regs_ETCNTINIT 0x0000000F 0x0000 R EPwm1Regs_DCTRIPSEL 0x0000000F 0x0043 R EPwm1Regs_DCACTL 0x0000000F 0x0000 R EPwm1Regs_DCBCTL 0x0000000F 0x0000 R EPwm1Regs_DCFCTL 0x0000000F 0x0000 R EPwm1Regs_DCCAPCTL 0x0000000F 0x0000 R EPwm1Regs_DCFOFFSET 0x0000000F 0x0000 R EPwm1Regs_DCFOFFSETCNT 0x0000000F 0x0000 R EPwm1Regs_DCFWINDOW 0x0000000F 0x0000 R EPwm1Regs_DCFWINDOWCNT 0x0000000F 0x0000 R EPwm1Regs_DCCAP 0x0000000F 0x0000 R EPwm1Regs_DCAHTRIPSEL 0x0000000F 0x0000 R EPwm1Regs_DCALTRIPSEL 0x0000000F 0x0000 R EPwm1Regs_DCBHTRIPSEL 0x0000000F 0x0000 R EPwm1Regs_DCBLTRIPSEL 0x0000000F 0x0000