This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
We are facing some issues with lab 12 ( encoder).
1- At start up, the motor starts some back and forth movements for few seconds and then starts moving normally. How can we fix this issue? RS calib and force_angle are both enabled.
2- Sometimes when we start spinning using CCS, motor spins in the reverse direction. why is that happening?
3- Also we have noticed that sometimes the motor does not respond to the speed commands or it takes a long time to change the speed after setting commands.
4- there is a huge overshoot when we change the speed. Does this have to do with PID coefficient? We have already tuned the bandwidth.
We have used the appropriate labs to detect motor parameters and configure the encoder. Any suggestions/comments on these issues will be highly appreciated.
The one more thing you need to check is an align current. In this lab, rotor is aligned to zero angle position before start up by using Rs recalculation function. But if rotor does not move to zero position due to the high load torque, PMSM motors do not work properly.
Please check if the Rs recalculation current(USER_MOTOR_RES_EST_CURRENT) is enough for moving rotor to electrically zero angle position.
Hi Steve,
Thank you for your input. Please see the waveforms for the encoder which seems to be clean and also the phase current at max speed. also increasing USER_MOTOR_RES_EST_CURRENT didn't help.
Let me just add that we have one more issue which is the maximum speed which is limited to about 400 rpm where and does not go beyond that number. Actually we have tested this motor before with sensorless and we were able to go to 700 rpm. ( the rated speed of our motor is 800 rpm, voltage: 48VDC, bldc motor, 8 pair poles). What's happening at high speed is that the motor phase current goes to high (40 arms)and motor gets too hot and stops working. The input current from power supply at max speed is about 12A at 48 VDC which is really high for the little load that we have which makes think that we are injecting some unnecessary id due to wrong offset of encoders maybe? note that enable force angle and enableoffsetcalc were both enabled in our testing. Also we tried to increase the input DC voltage to see if it makes change but it didn't help. Any idea why our motor speeds is limited? we are trying to find out why the motor is drawing too much power! We areally appreciate your URGENT help on this.
I think the encoder setting "USER_MOTOR_ENCODER_LINES" in user.h has some issue. You need to carefully check the encoder resolution spec. For example, the resolution in the encoder below is the value of post-quadrature. It means that the resolution(counts/rev) should be divide by 4 for USER_MOTOR_ENCODER_LINES because this lab use eQEP feature with quadrature enabled.
Could you share your encoder specification?
What the value of USER_MOTOR_ENCODER_LINES ?
Hi Steve, Thanks again for your support and helping us on this issue which is highly appreciated. We agree that there might be an issue with the encoder settings but not with the USER_MOTOR_ENCODER_LINES. The motor encoder CPR is 2500. So are you saying that we should try 2500/4 =625 ?
What about encoder offset? How do we make sure the encoder offset is correct?
And what does this number stand for ? #define ENC_ZERO_OFFSET 3813071.0
Thanks
if there is no any comment like "post-quad" on encoder , USER_MOTOR_ENCODER_LINES is 2500.
The define "ENC_ZERO_OFFSET" is not used as a constant in code. Instead, the enc zero offset is calculated by forcing align to electrical zero posing through Rs recalculation function such as the code in mainISR() below.
// if we are forcing alignment, using the Rs Recalculation, align the eQEP angle with the rotor angle
if((EST_getState(obj->estHandle) == EST_State_Rs) && (USER_MOTOR_TYPE == MOTOR_Type_Pm))
{
ENC_setZeroOffset(encHandle, (uint32_t)(HAL_getQepPosnMaximum(halHandle) - HAL_getQepPosnCounts(halHandle)));
gEnc_offset = HAL_getQepPosnCounts(halHandle);
}
I’m still doubt if encoder feedback does not have noise.
Could you check an encoder feedback again by running open-loop angle generation? You can add some data logging module, and can check encode count value or electrical angle while running motor with constant frequency and constant current with open-loop angle generation.
Did you check the encoder count direction by any chance?
A1 A2) . the attached file is for open loop test, and has data logging module for graph. please find the following test procedure.
step1. replace the origital proj_lab12b.c file with the attached file (proj_lab_12b_1.c).
step2. add "sw\modules\angle_gen\src\32\bangle_gen.c" file into the project
step3. compile & downloading & run
step4. gMotorVars.Flag_enableSys = 1
step5. gMotorVars.Flag_Run_Identify = 1
step6. Set target speed (gMotorVars.SpeedRef_krpm)
if gMotorVars.EstState becomes EST_State_Online, set the target speed with "gMotorVars.SpeedRef_krpm". 10~30% of rated speed is enough for this encoder test. You can increase Id current with gMotorVars.IdRef_A if you need more current for more high speed. The default value of Id reference current is same with Rs estimation current.
step6. Data logging enable (Graph_Flag_Enable_update = 1) once rotor reach to the target speed.
step7. Check encoder data by using CCS graph tool. Graph setting is as following.
The sample of test result should be like this. Electrical angle from encoder have to be positive direction and same frequency with phase current.
A3) Because an incremental encoder is just used in this lab, the offset is automatically calculated through forced align to zero angle. Generally, if encoder angle is not aligned with rotor angle, more current will need for torque output.
A4) Index signal is not used in this lab.
/* --COPYRIGHT--,BSD * Copyright (c) 2012, LineStream Technologies Incorporated * Copyright (c) 2012, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the names of Texas Instruments Incorporated, LineStream * Technologies Incorporated, nor the names of its contributors may be * used to endorse or promote products derived from this software without * specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * --/COPYRIGHT--*/ //! \file solutions/instaspin_motion/src/proj_lab12b.c //! \brief SpinTAC Velocity Controller using a quadrature encoder for feedback //! //! (C) Copyright 2012, LineStream Technologies, Inc. //! (C) Copyright 2011, Texas Instruments, Inc. //! \defgroup PROJ_LAB12b PROJ_LAB12b //@{ //! \defgroup PROJ_LAB12b_OVERVIEW Project Overview //! //! SpinTAC Velocity Controller using a quadrature encoder for feedback //! // ************************************************************************** // the includes // system includes #include <math.h> #include "main.h" #ifdef FLASH #pragma CODE_SECTION(mainISR,"ramfuncs"); #endif // Include header files used in the main function // ************************************************************************** // the defines #define LED_BLINK_FREQ_Hz 5 #define _GRAPH_ // ************************************************************************** // the globals uint_least16_t gCounter_updateGlobals = 0; bool Flag_Latch_softwareUpdate = true; CTRL_Handle ctrlHandle; HAL_Handle halHandle; USER_Params gUserParams; HAL_PwmData_t gPwmData = {_IQ(0.0), _IQ(0.0), _IQ(0.0)}; HAL_AdcData_t gAdcData; _iq gMaxCurrentSlope = _IQ(0.0); #ifdef FAST_ROM_V1p6 CTRL_Obj *controller_obj; #else CTRL_Obj ctrl; //v1p7 format #endif ENC_Handle encHandle; ENC_Obj enc; SLIP_Handle slipHandle; SLIP_Obj slip; ST_Obj st_obj; ST_Handle stHandle; uint16_t gLEDcnt = 0; volatile MOTOR_Vars_t gMotorVars = MOTOR_Vars_INIT; #ifdef FLASH // Used for running BackGround in flash, and ISR in RAM extern uint16_t *RamfuncsLoadStart, *RamfuncsLoadEnd, *RamfuncsRunStart; #endif #ifdef DRV8301_SPI // Watch window interface to the 8301 SPI DRV_SPI_8301_Vars_t gDrvSpi8301Vars; #endif #ifdef DRV8305_SPI // Watch window interface to the 8305 SPI DRV_SPI_8305_Vars_t gDrvSpi8305Vars; #endif _iq gFlux_pu_to_Wb_sf; _iq gFlux_pu_to_VpHz_sf; _iq gTorque_Ls_Id_Iq_pu_to_Nm_sf; _iq gTorque_Flux_Iq_pu_to_Nm_sf; uint32_t gEnc_offset = 0; #ifdef _GRAPH_ // Graphing Variables volatile bool Graph_Flag_Enable_update = false; volatile unsigned int Graph_Counter = 0; volatile unsigned short Graph_Tick_Counter = 0; volatile unsigned short Graph_Tick_Counter_Value = 5; #define GRAPH_SIZE 500 volatile _iq Graph_Data1[GRAPH_SIZE]; volatile _iq Graph_Data2[GRAPH_SIZE]; volatile _iq SpeedRef_krpm_previous = _IQ(0.0); #endif // define Angle Generate ANGLE_GEN_Handle angle_genHandle; ANGLE_GEN_Obj angle_gen; bool gFlag_IF_OpenLoop = false; // ************************************************************************** // the functions void main(void) { uint_least8_t estNumber = 0; #ifdef FAST_ROM_V1p6 uint_least8_t ctrlNumber = 0; #endif // Only used if running from FLASH // Note that the variable FLASH is defined by the project #ifdef FLASH // Copy time critical code and Flash setup code to RAM // The RamfuncsLoadStart, RamfuncsLoadEnd, and RamfuncsRunStart // symbols are created by the linker. Refer to the linker files. memCopy((uint16_t *)&RamfuncsLoadStart,(uint16_t *)&RamfuncsLoadEnd,(uint16_t *)&RamfuncsRunStart); #endif // initialize the hardware abstraction layer halHandle = HAL_init(&hal,sizeof(hal)); // check for errors in user parameters USER_checkForErrors(&gUserParams); // store user parameter error in global variable gMotorVars.UserErrorCode = USER_getErrorCode(&gUserParams); // do not allow code execution if there is a user parameter error if(gMotorVars.UserErrorCode != USER_ErrorCode_NoError) { for(;;) { gMotorVars.Flag_enableSys = false; } } // initialize the user parameters USER_setParams(&gUserParams); // set the hardware abstraction layer parameters HAL_setParams(halHandle,&gUserParams); // initialize the controller #ifdef FAST_ROM_V1p6 ctrlHandle = CTRL_initCtrl(ctrlNumber, estNumber); //v1p6 format (06xF and 06xM devices) controller_obj = (CTRL_Obj *)ctrlHandle; #else ctrlHandle = CTRL_initCtrl(estNumber,&ctrl,sizeof(ctrl)); //v1p7 format default #endif { CTRL_Version version; // get the version number CTRL_getVersion(ctrlHandle,&version); gMotorVars.CtrlVersion = version; } // set the default controller parameters CTRL_setParams(ctrlHandle,&gUserParams); // setup faults HAL_setupFaults(halHandle); // initialize the interrupt vector table HAL_initIntVectorTable(halHandle); // enable the ADC interrupts HAL_enableAdcInts(halHandle); // disable the PWM HAL_disablePwm(halHandle); // initialize the ENC module encHandle = ENC_init(&enc, sizeof(enc)); // setup the ENC module ENC_setup(encHandle, 1, USER_MOTOR_NUM_POLE_PAIRS, USER_MOTOR_ENCODER_LINES, 0, USER_IQ_FULL_SCALE_FREQ_Hz, USER_ISR_FREQ_Hz, 8000.0); // initialize the SLIP module slipHandle = SLIP_init(&slip, sizeof(slip)); // setup the SLIP module SLIP_setup(slipHandle, _IQ(gUserParams.ctrlPeriod_sec)); // initialize the SpinTAC Components stHandle = ST_init(&st_obj, sizeof(st_obj)); // initialize the angle generate module angle_genHandle = ANGLE_GEN_init(&angle_gen,sizeof(angle_gen)); ANGLE_GEN_setParams(angle_genHandle, gUserParams.iqFullScaleFreq_Hz, gUserParams.ctrlPeriod_sec); // setup the SpinTAC Components ST_setupVelCtl(stHandle); ST_setupPosConv(stHandle); #ifdef DRV8301_SPI // turn on the DRV8301 if present HAL_enableDrv(halHandle); // initialize the DRV8301 interface HAL_setupDrvSpi(halHandle,&gDrvSpi8301Vars); #endif #ifdef DRV8305_SPI // turn on the DRV8305 if present HAL_enableDrv(halHandle); // initialize the DRV8305 interface HAL_setupDrvSpi(halHandle,&gDrvSpi8305Vars); #endif // enable DC bus compensation CTRL_setFlag_enableDcBusComp(ctrlHandle, true); // compute scaling factors for flux and torque calculations gFlux_pu_to_Wb_sf = USER_computeFlux_pu_to_Wb_sf(); gFlux_pu_to_VpHz_sf = USER_computeFlux_pu_to_VpHz_sf(); gTorque_Ls_Id_Iq_pu_to_Nm_sf = USER_computeTorque_Ls_Id_Iq_pu_to_Nm_sf(); gTorque_Flux_Iq_pu_to_Nm_sf = USER_computeTorque_Flux_Iq_pu_to_Nm_sf(); // init variables gMotorVars.SpeedRef_krpm = _IQ(0.0); gMotorVars.IdRef_A = _IQ(USER_MOTOR_RES_EST_CURRENT); // enable global interrupts HAL_enableGlobalInts(halHandle); // enable debug interrupts HAL_enableDebugInt(halHandle); for(;;) { // Waiting for enable system flag to be set while(!(gMotorVars.Flag_enableSys)); // Dis-able the Library internal PI. Iq has no reference now CTRL_setFlag_enableSpeedCtrl(ctrlHandle, false); // loop while the enable system flag is true while(gMotorVars.Flag_enableSys) { CTRL_Obj *obj = (CTRL_Obj *)ctrlHandle; ST_Obj *stObj = (ST_Obj *)stHandle; // increment counters gCounter_updateGlobals++; // enable/disable the use of motor parameters being loaded from user.h CTRL_setFlag_enableUserMotorParams(ctrlHandle,gMotorVars.Flag_enableUserParams); // enable/disable Rs recalibration during motor startup EST_setFlag_enableRsRecalc(obj->estHandle,gMotorVars.Flag_enableRsRecalc); // enable/disable automatic calculation of bias values CTRL_setFlag_enableOffset(ctrlHandle,gMotorVars.Flag_enableOffsetcalc); if(CTRL_isError(ctrlHandle)) { // set the enable controller flag to false CTRL_setFlag_enableCtrl(ctrlHandle,false); // set the enable system flag to false gMotorVars.Flag_enableSys = false; // disable the PWM HAL_disablePwm(halHandle); } else { // update the controller state bool flag_ctrlStateChanged = CTRL_updateState(ctrlHandle); // enable or disable the control CTRL_setFlag_enableCtrl(ctrlHandle, gMotorVars.Flag_Run_Identify); if(flag_ctrlStateChanged) { CTRL_State_e ctrlState = CTRL_getState(ctrlHandle); if(ctrlState == CTRL_State_OffLine) { // enable the PWM HAL_enablePwm(halHandle); } else if(ctrlState == CTRL_State_OnLine) { if(gMotorVars.Flag_enableOffsetcalc == true) { // update the ADC bias values HAL_updateAdcBias(halHandle); } else { // set the current bias HAL_setBias(halHandle,HAL_SensorType_Current,0,_IQ(I_A_offset)); HAL_setBias(halHandle,HAL_SensorType_Current,1,_IQ(I_B_offset)); HAL_setBias(halHandle,HAL_SensorType_Current,2,_IQ(I_C_offset)); // set the voltage bias HAL_setBias(halHandle,HAL_SensorType_Voltage,0,_IQ(V_A_offset)); HAL_setBias(halHandle,HAL_SensorType_Voltage,1,_IQ(V_B_offset)); HAL_setBias(halHandle,HAL_SensorType_Voltage,2,_IQ(V_C_offset)); } // Return the bias value for currents gMotorVars.I_bias.value[0] = HAL_getBias(halHandle,HAL_SensorType_Current,0); gMotorVars.I_bias.value[1] = HAL_getBias(halHandle,HAL_SensorType_Current,1); gMotorVars.I_bias.value[2] = HAL_getBias(halHandle,HAL_SensorType_Current,2); // Return the bias value for voltages gMotorVars.V_bias.value[0] = HAL_getBias(halHandle,HAL_SensorType_Voltage,0); gMotorVars.V_bias.value[1] = HAL_getBias(halHandle,HAL_SensorType_Voltage,1); gMotorVars.V_bias.value[2] = HAL_getBias(halHandle,HAL_SensorType_Voltage,2); // enable the PWM HAL_enablePwm(halHandle); } else if(ctrlState == CTRL_State_Idle) { // disable the PWM HAL_disablePwm(halHandle); gMotorVars.Flag_Run_Identify = false; gFlag_IF_OpenLoop = false; angle_gen.Angle_pu = _IQ(0.0); } if((CTRL_getFlag_enableUserMotorParams(ctrlHandle) == true) && (ctrlState > CTRL_State_Idle) && (gMotorVars.CtrlVersion.minor == 6)) { // call this function to fix 1p6 USER_softwareUpdate1p6(ctrlHandle); } } } if(EST_isMotorIdentified(obj->estHandle)) { // set the current ramp EST_setMaxCurrentSlope_pu(obj->estHandle,gMaxCurrentSlope); gMotorVars.Flag_MotorIdentified = true; // set the speed reference CTRL_setSpd_ref_krpm(ctrlHandle,gMotorVars.SpeedRef_krpm); // set the speed acceleration CTRL_setMaxAccel_pu(ctrlHandle,_IQmpy(MAX_ACCEL_KRPMPS_SF,gMotorVars.MaxAccel_krpmps)); // enable the SpinTAC Speed Controller STVELCTL_setEnable(stObj->velCtlHandle, true); if(EST_getState(obj->estHandle) != EST_State_OnLine) { // if the estimator is not running, place SpinTAC into reset STVELCTL_setEnable(stObj->velCtlHandle, false); } else { gFlag_IF_OpenLoop = true; } if(Flag_Latch_softwareUpdate) { Flag_Latch_softwareUpdate = false; USER_calcPIgains(ctrlHandle); // initialize the watch window kp and ki current values with pre-calculated values gMotorVars.Kp_Idq = CTRL_getKp(ctrlHandle,CTRL_Type_PID_Id); gMotorVars.Ki_Idq = CTRL_getKi(ctrlHandle,CTRL_Type_PID_Id); // initialize the watch window Bw value with the default value gMotorVars.SpinTAC.VelCtlBw_radps = STVELCTL_getBandwidth_radps(stObj->velCtlHandle); // initialize the watch window with maximum and minimum Iq reference gMotorVars.SpinTAC.VelCtlOutputMax_A = _IQmpy(STVELCTL_getOutputMaximum(stObj->velCtlHandle), _IQ(USER_IQ_FULL_SCALE_CURRENT_A)); gMotorVars.SpinTAC.VelCtlOutputMin_A = _IQmpy(STVELCTL_getOutputMinimum(stObj->velCtlHandle), _IQ(USER_IQ_FULL_SCALE_CURRENT_A)); } } else { Flag_Latch_softwareUpdate = true; // the estimator sets the maximum current slope during identification gMaxCurrentSlope = EST_getMaxCurrentSlope_pu(obj->estHandle); } // when appropriate, update the global variables if(gCounter_updateGlobals >= NUM_MAIN_TICKS_FOR_GLOBAL_VARIABLE_UPDATE) { // reset the counter gCounter_updateGlobals = 0; updateGlobalVariables_motor(ctrlHandle, stHandle); } // update Kp and Ki gains updateKpKiGains(ctrlHandle); // set the SpinTAC (ST) bandwidth scale STVELCTL_setBandwidth_radps(stObj->velCtlHandle, gMotorVars.SpinTAC.VelCtlBw_radps); // set the maximum and minimum values for Iq reference STVELCTL_setOutputMaximums(stObj->velCtlHandle, _IQmpy(gMotorVars.SpinTAC.VelCtlOutputMax_A, _IQ(1.0/USER_IQ_FULL_SCALE_CURRENT_A)), _IQmpy(gMotorVars.SpinTAC.VelCtlOutputMin_A, _IQ(1.0/USER_IQ_FULL_SCALE_CURRENT_A))); // enable/disable the forced angle EST_setFlag_enableForceAngle(obj->estHandle,gMotorVars.Flag_enableForceAngle); // enable or disable power warp CTRL_setFlag_enablePowerWarp(ctrlHandle,gMotorVars.Flag_enablePowerWarp); #ifdef DRV8301_SPI HAL_writeDrvData(halHandle,&gDrvSpi8301Vars); HAL_readDrvData(halHandle,&gDrvSpi8301Vars); #endif #ifdef DRV8305_SPI HAL_writeDrvData(halHandle,&gDrvSpi8305Vars); HAL_readDrvData(halHandle,&gDrvSpi8305Vars); #endif } // end of while(gFlag_enableSys) loop // disable the PWM HAL_disablePwm(halHandle); // set the default controller parameters (Reset the control to re-identify the motor) CTRL_setParams(ctrlHandle,&gUserParams); gMotorVars.Flag_Run_Identify = false; // setup the SpinTAC Components ST_setupVelCtl(stHandle); ST_setupPosConv(stHandle); } // end of for(;;) loop } // end of main() function interrupt void mainISR(void) { static uint16_t stCnt = 0; CTRL_Obj *obj = (CTRL_Obj *)ctrlHandle; _iq angle_pu = 0; // toggle status LED if(++gLEDcnt >= (uint_least32_t)(USER_ISR_FREQ_Hz / LED_BLINK_FREQ_Hz)) { HAL_toggleLed(halHandle,(GPIO_Number_e)HAL_Gpio_LED2); gLEDcnt = 0; } // compute the electrical angle ENC_calcElecAngle(encHandle, HAL_getQepPosnCounts(halHandle)); // acknowledge the ADC interrupt HAL_acqAdcInt(halHandle,ADC_IntNumber_1); // convert the ADC data HAL_readAdcData(halHandle,&gAdcData); // Run the SpinTAC Components if(stCnt++ >= ISR_TICKS_PER_SPINTAC_TICK) { ST_runPosConv(stHandle, encHandle, ctrlHandle); ST_runVelCtl(stHandle, ctrlHandle); stCnt = 1; } // open-loop angle generation if(gFlag_IF_OpenLoop) { _iq speed_ref_pu = TRAJ_getIntValue(controller_obj->trajHandle_spd); ANGLE_GEN_run(angle_genHandle, speed_ref_pu); // generate the motor electrical angle angle_pu = ANGLE_GEN_getAngle_pu(angle_genHandle); } if(USER_MOTOR_TYPE == MOTOR_Type_Induction) { // update the electrical angle for the SLIP module SLIP_setElectricalAngle(slipHandle, ENC_getElecAngle(encHandle)); // compute the amount of slip SLIP_run(slipHandle); // run the controller CTRL_run(ctrlHandle,halHandle,&gAdcData,&gPwmData,SLIP_getMagneticAngle(slipHandle)); } else { if(gFlag_IF_OpenLoop) { // run the controller with open-loop angle CTRL_run(ctrlHandle,halHandle,&gAdcData,&gPwmData,angle_pu); } else { // run the controller CTRL_run(ctrlHandle,halHandle,&gAdcData,&gPwmData,ENC_getElecAngle(encHandle)); } } // write the PWM compare values HAL_writePwmData(halHandle,&gPwmData); // setup the controller CTRL_setup(ctrlHandle); // if we are forcing alignment, using the Rs Recalculation, align the eQEP angle with the rotor angle if((EST_getState(obj->estHandle) == EST_State_Rs) && (USER_MOTOR_TYPE == MOTOR_Type_Pm)) { ENC_setZeroOffset(encHandle, (uint32_t)(HAL_getQepPosnMaximum(halHandle) - HAL_getQepPosnCounts(halHandle))); gEnc_offset = HAL_getQepPosnCounts(halHandle); } #ifdef _GRAPH_ // store graph value if(Graph_Flag_Enable_update) { if(Graph_Counter >= GRAPH_SIZE) { Graph_Flag_Enable_update = false; Graph_Counter = 0; } else { if(Graph_Tick_Counter == 0) { Graph_Data1[Graph_Counter] = gAdcData.I.value[0]; //Ia Graph_Data2[Graph_Counter] = ENC_getElecAngle(encHandle); //elec_angle; Graph_Counter++; Graph_Tick_Counter = Graph_Tick_Counter_Value - 1; } else { Graph_Tick_Counter--; } } } #endif return; } // end of mainISR() function void updateGlobalVariables_motor(CTRL_Handle handle, ST_Handle sthandle) { CTRL_Obj *obj = (CTRL_Obj *)handle; ST_Obj *stObj = (ST_Obj *)sthandle; // get the speed estimate gMotorVars.Speed_krpm = EST_getSpeed_krpm(obj->estHandle); // get the speed from eQEP gMotorVars.SpeedQEP_krpm = _IQmpy(STPOSCONV_getVelocityFiltered(stObj->posConvHandle), _IQ(ST_SPEED_KRPM_PER_PU)); // get the real time speed reference coming out of the speed trajectory generator gMotorVars.SpeedTraj_krpm = _IQmpy(CTRL_getSpd_int_ref_pu(handle),EST_get_pu_to_krpm_sf(obj->estHandle)); // get the torque estimate gMotorVars.Torque_Nm = USER_computeTorque_Nm(handle, gTorque_Flux_Iq_pu_to_Nm_sf, gTorque_Ls_Id_Iq_pu_to_Nm_sf); // get the magnetizing current gMotorVars.MagnCurr_A = EST_getIdRated(obj->estHandle); // get the rotor resistance gMotorVars.Rr_Ohm = EST_getRr_Ohm(obj->estHandle); // get the stator resistance gMotorVars.Rs_Ohm = EST_getRs_Ohm(obj->estHandle); // get the stator inductance in the direct coordinate direction gMotorVars.Lsd_H = EST_getLs_d_H(obj->estHandle); // get the stator inductance in the quadrature coordinate direction gMotorVars.Lsq_H = EST_getLs_q_H(obj->estHandle); // get the flux in V/Hz in floating point gMotorVars.Flux_VpHz = EST_getFlux_VpHz(obj->estHandle); // get the flux in Wb in fixed point gMotorVars.Flux_Wb = USER_computeFlux(handle, gFlux_pu_to_Wb_sf); // get the controller state gMotorVars.CtrlState = CTRL_getState(handle); // get the estimator state gMotorVars.EstState = EST_getState(obj->estHandle); // Get the DC buss voltage gMotorVars.VdcBus_kV = _IQmpy(gAdcData.dcBus,_IQ(USER_IQ_FULL_SCALE_VOLTAGE_V/1000.0)); // get the Iq reference from the speed controller gMotorVars.IqRef_A = _IQmpy(STVELCTL_getTorqueReference(stObj->velCtlHandle), _IQ(USER_IQ_FULL_SCALE_CURRENT_A)); // read Id and Iq vectors in amps gMotorVars.Id_A = _IQmpy(CTRL_getId_in_pu(ctrlHandle), _IQ(USER_IQ_FULL_SCALE_CURRENT_A)); gMotorVars.Iq_A = _IQmpy(CTRL_getIq_in_pu(ctrlHandle), _IQ(USER_IQ_FULL_SCALE_CURRENT_A)); // calculate vector Is in amps gMotorVars.Is_A = _IQsqrt(_IQmpy(gMotorVars.Id_A, gMotorVars.Id_A) + _IQmpy(gMotorVars.Iq_A, gMotorVars.Iq_A)); // gets the Velocity Controller status gMotorVars.SpinTAC.VelCtlStatus = STVELCTL_getStatus(stObj->velCtlHandle); // get the inertia setting gMotorVars.SpinTAC.InertiaEstimate_Aperkrpm = _IQmpy(STVELCTL_getInertia(stObj->velCtlHandle), _IQ(ST_SPEED_PU_PER_KRPM * USER_IQ_FULL_SCALE_CURRENT_A)); // get the friction setting gMotorVars.SpinTAC.FrictionEstimate_Aperkrpm = _IQmpy(STVELCTL_getFriction(stObj->velCtlHandle), _IQ(ST_SPEED_PU_PER_KRPM * USER_IQ_FULL_SCALE_CURRENT_A)); // get the Velocity Controller error gMotorVars.SpinTAC.VelCtlErrorID = STVELCTL_getErrorID(stObj->velCtlHandle); // get the Position Converter error gMotorVars.SpinTAC.PosConvErrorID = STPOSCONV_getErrorID(stObj->posConvHandle); return; } // end of updateGlobalVariables_motor() function void updateKpKiGains(CTRL_Handle handle) { if((gMotorVars.CtrlState == CTRL_State_OnLine) && (gMotorVars.Flag_MotorIdentified == true) && (Flag_Latch_softwareUpdate == false)) { // set the kp and ki speed values from the watch window CTRL_setKp(handle,CTRL_Type_PID_spd,gMotorVars.Kp_spd); CTRL_setKi(handle,CTRL_Type_PID_spd,gMotorVars.Ki_spd); // set the kp and ki current values for Id and Iq from the watch window CTRL_setKp(handle,CTRL_Type_PID_Id,gMotorVars.Kp_Idq); CTRL_setKi(handle,CTRL_Type_PID_Id,gMotorVars.Ki_Idq); CTRL_setKp(handle,CTRL_Type_PID_Iq,gMotorVars.Kp_Idq); CTRL_setKi(handle,CTRL_Type_PID_Iq,gMotorVars.Ki_Idq); } return; } // end of updateKpKiGains() function void ST_runPosConv(ST_Handle handle, ENC_Handle encHandle, CTRL_Handle ctrlHandle) { ST_Obj *stObj = (ST_Obj *)handle; // get the electrical angle from the ENC module STPOSCONV_setElecAngle_erev(stObj->posConvHandle, ENC_getElecAngle(encHandle)); if(USER_MOTOR_TYPE == MOTOR_Type_Induction) { // The CurrentVector feedback is only needed for ACIM // get the vector of the direct/quadrature current input vector values from CTRL STPOSCONV_setCurrentVector(stObj->posConvHandle, CTRL_getIdq_in_addr(ctrlHandle)); } // run the SpinTAC Position Converter STPOSCONV_run(stObj->posConvHandle); if(USER_MOTOR_TYPE == MOTOR_Type_Induction) { // The Slip Velocity is only needed for ACIM // update the slip velocity in electrical angle per second, Q24 SLIP_setSlipVelocity(slipHandle, STPOSCONV_getSlipVelocity(stObj->posConvHandle)); } } void ST_runVelCtl(ST_Handle handle, CTRL_Handle ctrlHandle) { _iq speedFeedback, iqReference; ST_Obj *stObj = (ST_Obj *)handle; CTRL_Obj *ctrlObj = (CTRL_Obj *)ctrlHandle; // Get the mechanical speed in pu speedFeedback = STPOSCONV_getVelocityFiltered(stObj->posConvHandle); // Run the SpinTAC Controller // Note that the library internal ramp generator is used to set the speed reference STVELCTL_setVelocityReference(stObj->velCtlHandle, TRAJ_getIntValue(ctrlObj->trajHandle_spd)); STVELCTL_setAccelerationReference(stObj->velCtlHandle, _IQ(0.0)); // Internal ramp generator does not provide Acceleration Reference STVELCTL_setVelocityFeedback(stObj->velCtlHandle, speedFeedback); STVELCTL_run(stObj->velCtlHandle); // select SpinTAC Velocity Controller iqReference = STVELCTL_getTorqueReference(stObj->velCtlHandle); // Set the Iq reference that came out of SpinTAC Velocity Control CTRL_setIq_ref_pu(ctrlHandle, iqReference); if(gFlag_IF_OpenLoop) { CTRL_setIq_ref_pu(ctrlHandle, _IQ(0.0)); CTRL_setId_ref_pu(ctrlHandle, _IQmpy(gMotorVars.IdRef_A, _IQ(1.0/USER_IQ_FULL_SCALE_CURRENT_A))); } } //@} //defgroup // end of file
I'm wondering why the open-loop test code is not working. If you are using DRV8301-69M-KIT without any modification, this code should work. Did you check the motor A-phase current with oscilloscope? If you’ve done setup properly your motor parameters in user.h, you can see an align current at start-up and rotating current while motor running.
The reason I provided the test code is that I wanted to confirm two things: the encoder signal integrity, the direction of encoder angle. The encoder angle have to be same direction with rotating flux. For example, if rotor is running with positive torque, the direction of encoder angle have to be up-count like the waveform I attached on above answer.
Can you attach your user.h file for checking your motor parameters and board settings?
I'm sorry to hear that your kit was damaged. I hope you have extra new one.
I think your motor phase and encoder pulse direction are not matched. If so, you can resolve the issue by simply exchanging the encoder A/B connection each other or exchanging only the motor two phases connection(U<->V or U<->W or V<->W).
phase current waveform.docxI have also attached the Phase current waveform at max speed when it starts oscillating
Steve,
I have also attached the motor datasheet for your reference. The maximum speed is 800rpm. As mentioned, we cannot go above almost 500 rpm. we don't have the motor characteristics to see what we should expect from the motor at high speed. Is this normal that for a rated 800 rpm motor, you can't get a higher rpm than 500 ?
Hi Steve,
We had tried the values that you suggested. In fact, we started with those values and the maximum rpm we get using those values is 360 rpm. increasing #define USER_MOTOR_MAX_CURRENT from 10 to 20 helped to get up to 500 rpm. After that, increasing max current didn't help. Increasing input voltage didn't help either. Do you think we are hitting the maximum power this motor can handle? also do you think field weakening or over modulation might help?