Hi,
I am opening a related thread for the same topic since the last one has been locked.
I still haven't got a clear feedback on this matter, but I suppose ARM also didn't give any feedback on this Errata ; however I would really appreciate an answer to confirm the use of WB policy for cache memory on R5.
Here is the original question :
The errata CORTEX-R5#7 (ARM ID-780125) suggests a work-around to avoid deadlock or data loss when using cache-ECC: setting the ACTLR.DBWR bit to 1.
It is unclear to me if additionnally to this work-around, the write-back attribute should or should not be used for the different memory regions of the TMS.
It is written that "This setting also disables generation of AXI bursts by the processor for Write-Through and Non-cacheable Normal memory, but not Write-Back memory."
So can I use the write-back attribute for SRAM, external memories, etc. ? or am I forced to use write-through attribute (which reduces significantly the performance of the cache) ?
It is confusing for me that the issue starts with "When Write-back cache is selected..." (so this mode seems to be the issue) and that the workaround paragraph explains the DBWR does not disable the AXI bursts for Write-back.
I really need to be sure if I can or cannot use the Write-back mode at all when the workaround is applied...
Thank you,
Regards,
RP