This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi MSP430 fans,
I have just forked the TI MSP430 USB Firmware Updater as a Visual Studio 2019 Solution on GitHub :
https://github.com/Howerd/MSP430_USB_Firmware_Updater
The modifications include the ability to upload firmware from a TI TXT file with more than one @XXXX address command line, and a simpler user interface.
I am posting this here in case it is useful for anyone who wishes to program a MSP430F5529 chip - it should also work with any similar chips with up to 256K bytes of FLASH memory starting at 0x4400.
This program allows the target firmware to be updated using only a USB cable, instead of using a MSP-FET430UIF JTAG Interface.
Cheers,
Howerd
Hi Howerd,
Thank you for your great sharing!!!
Eason
Hi Eason,
No problem :-)
In fact, I did this upgrade to support a colleague in the UK - I had designed some hardware using the MSP430F5529 back in 2010 - he had problems programing the devices using Windows 10.
I still like the MSP430F55xx chips, especially the USB BSL feature - it is a really nice feature.
Cheers,
Howerd
Hi Howerd,
It is nice to hear that! We are still doing some update for the MSP430 content to make it easy for customers.
Eason
**Attention** This is a public forum