This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
no ports enumerated, win10, ccs 10, both updated, or win7, ccs 10 (separated machine) trying to debug msp-exp430f5529lp or msp-exp430fr4133. No USB FET was found and no comports enumerated in device manager.
these devices are more than a year old and have been used before with minimum problems
Hi Wally,
Ok, just to confirm, when either one is plugged into the PC with the device manager open, you don't see Windows activity detecting a USB device and refreshing OR updating the device manager window (the usual process Windows goes through when attaching a USB device)?
On the MSP-EXP430F5229 LP, if this is true and the green LED (near USB connector) is on, its possible the TUSB2046 USB HUB device located on the launchpad is faulty. But the MSP-EXP430FR4133 doesn't have the device, so I'm not sure what's up with that one.
To better understand the background, is the Win10 and Win7 PC the same ones used in the past successfully and if so, did you perform any updates/upgrades/changes recently?
When CCS is installed, the appropriate drivers are automatically installed so I would rule that out.
Here is my favorite question - did you try a different USB cable?
Hi Wally,
It's been a while since we have heard from you, so I'm going to assume you were able to move forward with your project.
I will mark this posting as RESOLVED, but if this isn’t the case, please click the "This did NOT resolve my issue" button and reply to this thread with more information.
If this thread is locked, please click the "Ask a related question" button, and in the new thread describe the current status of your issue and any additional details you may have to assist us in helping to solve your issues.
**Attention** This is a public forum