Part Number: MSP430G2755
Other Parts Discussed in Thread: MSP430FR2311, MSP-FET
Hi dear people,
my custom board with a MSP430G2755 should work with a supply of 1.8V.
Debugging and programming the device with the eZ-FET Emulator from the MSP430FR2311 oder similar Launchpad should be possible, following the information on SLAU664B,
However, I have two questions:
A: The XDS110 debuggers (which I cannot use) have level shifters to accommodate the voltages between board and emulator. I do not see them on the eZ-FET.
Are they not needed by the eZ-FET Emulator?
B: The datasheet of the MSP430G2755 says, that the recommended supply voltage during flash programming or erase should be min. 2.2V
Would it work with the 1.8V, or should I implement a way to increase the voltage during debugging/programming?
As usual I thank you for the help you always provide.
Best regards,
Gustavo