This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-FET: Writing cannot be performed normally with MSP-FET430UIF

Guru 10880 points
Part Number: MSP-FET
Other Parts Discussed in Thread: UNIFLASH

Hi,

Writing is done using the following debugger. When I use ① MSP-FET430UIF, I can't write software, but ② MSP-FET can write normally.

I'm using Uniflash to write, but I can't write with the error [Device not found].

 - Debugger ①: MSP-FET430UIF
 - Debugger ②: MSP-FET

The connection diagram between the board and the debugger is shown below.

Is it possible to get some advice?

Thanks,

Conor

**Attention** This is a public forum