Hi,
We are using the DCO at 8MHz on MSP430 and I am investigating whether it is possible to shift the DCO to 8.1MHz using the FR5043's functions. It seems that the FR4xx/FR2xx have a DCO trimming function that allows the frequency to be shifted. However, the FR5xx does not seem to have such a function.
- https://www.ti.com/lit/an/slaa992/slaa992.pdf
Do you have any ideas?
Thanks,
Conor