This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-FET: MSP-FET vs Ez-FET UART Backchannel

Part Number: MSP-FET


Tool/software:

I have been using Ez-FET for a long time and I now consider a switch to MSP-FET probe.

Ez-FET presents 2 separate USB interface, one for the debug interface and one for the UART channel.  That gives 2 COM ports named  "MSP debug interface" and "MSP application UART" at the descriptor level.  The application UART is actually a passthrough, which is very convenient.

Does the MSP-FET do the same as the Ez-FET  (2 interfaces) or its "backchannel UART " is somehow entangled with the debug interface all in one single USB interface that requires the appropriate driver+software to be used? 

Regards

**Attention** This is a public forum