This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Howdie,
I've only been playing with the MSP430 for a couple of weeks and seem to have gotten myself probably in a pickle. What I mean is, I was able to observe the demo software (the blinking leds and the temperature change indication demo by the led. Worked according to as described in your documentation. I di try to actually display the "Current Temperature" using the provided .jave GUI interface but was only half successful ... what I mean by this is while "Current Temperature" was displayed in an MS-DPS window the font of the text was so large I could actually see the temperature readings. I'm pretty sure a temperature reading was there as I think I could make outa shaved cahracter being displayed. LOL! BTW, all this was with the 14 pin chip in the socket.
Then I swapped to the 20 pin chip and played around with capacitive touch booster item. All good, but when I changed back to the 14 pin I wasn't ab;e to observe the original demos as described in the first paragraph. As far as I know, I didn't "intentionally" do any modification to any code (in facct, at this stage I don't know how to). But as we all know, "things happen" so I'll take the hit here.
So I would like to know where I can find the originally supplyed demo code so I can attempt to download/write to the 14 pin chip. Any help here would be appreciated!
Also when perusing the various source code folders (asm, c, java) I noticed different file extensions that I'm just not familiar with at all and searchs of the internet didn't result in any definitive answers. What the heck is a .pde file extension? Do the two IDEs (CCS and IAR) use a lot of different file extensions?
Hope I make some sort of sense here.
Thanks in advance,
Bo
Dirigo here,
Please ignore or delete this as I originally posted this on the wrong forum. Subsequently I reposted it on the correct forum and got response from two gentlemen who answered my original questions.
Sorry for any inconvenience I may have caused.
Dirio
**Attention** This is a public forum