This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

"MSP430: Can't Single Step Target Program: Could not single step device"

Hi, when I try to singelstep in CCE v4 I get this message "MSP430: Can't Single Step Target Program: Could not single step device", I don't really know why or how to fix this problem? To test that it was not my code I also have tested with an new project and sample code for the MCU I have, the programmer also has the newest firmware (it got updated before my first launch).

Anyone who can help me out here? [:)]

  • May be this post will help:
    http://e2e.ti.com/forums/t/844.aspx

    Also hopefully the firmware on your USB debugger is up to date.
    One thing that may be done: There is a free tool made by ELPROTRONIC (www.elprotronic.com) for the FET 430UIF. This tool also reflashes the FET430UIF if it is not the correct version to work with their software.

    Despite the error, are you able to put a breakpoint somewhere in the code and run it?
    I recommend the following:
    1. Create a brand new project using the following to make that the project settings are correct:
    https://community.ti.com/forums/t/65.aspx

    2. Use a TI Target board if possible to run this test:
    http://focus.ti.com/mcu/docs/mcuprodmsptoolsw.tsp?sectionId=95&tabId=1203&familyId=342&toolTypeId=1#FETkits

  • Well I'm sorry to say that this did not help that much... I followed the instructions and it still did not work, same problem, although I'm not using CCE v3, I use CCE v4. I have an brand new TI Target board an MSP-FET430u28. I guess I have to try out CCE v3 also since that program you liked to does not seam to work.

  • Good news, now it's working! I don't really know why but I installed CCE v3 and it updated the firmware (again, it was done in CCE v4 before) and after that it worked in CCE v3, after that I tried with CCE v4 again and then it started with updating the firmware (again) and after that it worked in CCE v4 as well! [:)]

    I guess maybe something got wrong when I updated the firmware the first time maybe, however now it works thanks for the tips anyway.

  • Hi, I have the same error. After i leave the interrupt vector it goes back to the end of GoToSleep function and pops up the error.

    void GoToSleep()
    {
    TA0CCR0 = 5; 
    TACCTL0 = CCIE; // CCR0 interrupt enabled
    TACTL = TASSEL_2 + MC_1;
    _BIS_SR(LPM0_bits + GIE); // Go to sleep in low power mode 0 , with interrupts enabled.
    }

    #pragma vector=TIMERA0_VECTOR
    __interrupt void Timer_A0(void)
    {
    PSU_ON(); // just a function for the LEDs
    CCR0 += 5; // Add Offset to CCR0
    PSU_OFF(); just a function for the LEDs
    }

    Any suggestions what might cause the problem?

    Thanks,

    Vasil

**Attention** This is a public forum