This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I use MSP-EXP430F5529 Experimenter board, I have seen the similar question on the forum but I can't find the solution from any of them.
I used USB of eZ430-EMULATION.
The problem is when I connected my card with PC, it said that it's a unknown device; when I built the latest User Experience by CCS 5.5.0, it said that "Error initializing emulator: No USB FET was found"
I have installed MSP-EXP430F5529_UE-1.31.00.00-Setup (but I am not sure if it's necessary).
Could you help me to solve this question?
Thanks a lot.
The Hub is an USB standard class device. So you don't need to install anything by your self. The driver will be automatically installed by your operating system.
Have you tried to connect the board to other USB ports?
If that doesn't help, my best recommendation is to return/replace your board.
Best Regards,
Mo.
Thanks I lot.
By the way, when I want to debug the experimenter board MSP-EXP430F5529, I have to connect the eZ430-EMULATION with the PC by the USB line with two USB connectors?
Haiqi Bian said:By the way, when I want to debug the experimenter board MSP-EXP430F5529, I have to connect the eZ430-EMULATION with the PC by the USB line with two USB connectors?
Sorry but I don't know what you mean by "USB line with two USB connectors". However, you have to use the original USB cable that was included in the MSP-EXP430F5529 box.
Regards,
Mo.
**Attention** This is a public forum