This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi experts,
I'm new to MSP430 development and have the Problem, that one of five MSP430F5529LP are not working any longer after attempting to debug the board with the latest CCS.
The following procedure worked for the first 4 boards, but unfortunately not for the fifth...
- On first debugging attempt CCS made a firmware update of the board
- CCS downloaded the program
- Tests with the usb cdc communication program succeeded
Only with the last (fifth) board the Firmware update failed somewhere in the middle and since, all communication through "MSP Debug Interface" is not possible for this board anymore.
I tried to start the board with the BSL but every attempt to communicate with the board failed (CCS, Elprotronic FET-Pro430, etc.)
Has anyone any experience on this subject?
Any idea whether it can be solved?
Do I need a new board?
Cheers
Rolf
Just in case someone ran into the same issue, Before spending money to buy MSP-FET (good to have though) try this first:
1. delete the drivers (MSP Debug Interface and MSP Application UART1)
2. then restart CCS, and replug in your MSP430F5529,
3. New drivers will be installed and it will prompt you to update the firmware for the debugger.
It worked for me, so it's worth the try before doing something more complicated.
-Cuong Dao
**Attention** This is a public forum