Other Parts Discussed in Thread: MSP-GANG
Hello,
I have only now arrive to a stage that I have time to fix the most annoying issue.
I get "Interface Communication Error" once in a while.
NOT after update of the msp430-usb-debug-interface.
Another point to issue is that many times we work with 3 JTAGs at once & only 1 of them dies with this BUG.
Another test that we have done was during evaluation of the IAR this bug DOESN'T OCCURS AT ALL when using the with the IAR for MSP430.
Moreover this happens with all our windows 7 PCs (more than 4, not all configures the same way).
Setup:
- PC OS - windows 74 Ultimate
- CCS - Version: 6.0.1.00040
- TI MSP - MSP430F54308
- JTAG - msp430 usb debug interface
I've read several post about this issue like this and others (with less detail)
The only working solutions we have at the moment:
- Replace the JTAG with different JTAG usually solves this.
- Reset the PC.
Both of these solution aren't OK, we would like to find the source for this issue so plz help us fix this BUG for good.
I would like to stress out that this doesn't happened after JTAG update and happens about 5-20+ times a month.