This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
I'm trying to program the MSP430FR6989 chip on a customized board through the MSP-FETFlash Emulation Tool. When I tried to flash my .out file in Uniflash, it shows me "No debug probes/devices detected".
The drivers have been installed, and I can also see 'MSP Application UART1' and "MSP Debug Interface" device in device manager. Whenever I plugged in my MSP430 programmer, Uniflash could sense it and did an auto-detect, but still no devices been detected.
I tried the "New Configuration" and manually chose my device and port. At the first start, the MSP-FET has been updated its own firmware, but when I continued flashing the .out file, it showed me that no devices detected error again. (so I believe it can recognize the MSP-FET but couldn't talk to the MSP430 chip)
My board was powered externally by a power supply. My operating system is Windows 10. JTAG is not likely to have a connection error.
Is it likely to have something wrong between the MSP-FET and the target MSP430 MCU? Any idea on how to debug this?
Thank you,
DL
Also the resistor and capacitors are next to JT1, which is about 2 inches from the MSP430.
Hello Shang,
Schematic looks okay to me. Do you have an EVM you can test with? That way you can figure out if it's a hardware issue or not.
Also, I'm going to be traveling for the next week so my responses will be very delayed. Someone else from the community may be able to assist.
Thanks,
JD
Hi JD,
Thank you very much for the replies. We found out the problem was due to a damaged HDMI cable. It causes the system sometimes works and sometimes doesn't. We were able to flash the firmware successfully with another HDMI cable.
Thanks,
Dongmeng
**Attention** This is a public forum