This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a MSP-GANG Programmer and I want use this device to unlock a MSP432 MCU which was locked by set JTAG_SWD_LOCK_SECEN.
I know use MSP-GANG window software can unlock it by click "Clear Locked Device" button .
But in this way , I need install the windows software.
I want just use the MSP-GANG device like the Standalone mode to unlock the MCU.
Is it possible that I make an image just do unlock the MCU process and download it into MSP-GANG?
Or any other ways to unlock the MCU just use the MSP-GANG device .
Thanks!
user1600444,
All protection options are described in the MSP432 Technical Reference Manual and are implemented by programming the flash mailbox. The MSP-GANG can program the flash mailbox according to user settings or directly from code file.
See Section 4.8 in the MSP432 TRM here.
BR,
Seong
**Attention** This is a public forum