This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: PWM Glitch with MSP432

Part Number: MSP432P401R

I'm trying to use relatively high frequency PWM on the MSP432 Timer A.  The PWM frequency is ~100kHz, and it's updated at a 20kHz rate, using the Systick interrupt.

It almost works, but the issue is that there is an occasional glitch in the duty cycle, probably when the duty cycle is updated.  This is fatal for my application, so I was wondering if there's a glitchless way to update the PWM duty cycle?  Or if that's not the issue what might be the root cause and solution? 

I note that the MSP432 doesn't seem to have the double-buffered compare register structure that is typically used to avoid this problem, so I'm hoping that there is some workaround other than switching to a different device.  Thanks!

The glitch:

The code:  (Sorry, I'm an analog/power hardware guy, so probably not too elegant!)

#include <ti/devices/msp432p4xx/driverlib/driverlib.h>
#include <ti/devices/msp432p4xx/inc/msp.h>
/* Standard Includes */
#include <stdint.h>
#include <stdbool.h>
#include <math.h>

static volatile uint32_t aclk, mclk, smclk, hsmclk, bclk;

#define CPU_F ((double)48000000)
#define TIMER_A0_MODULE 0X4000
#define delay_us(x) __delay_cycles((long)(CPU_F*(double)x/1000000.0))
#define delay_ms(x) __delay_cycles((long)(CPU_F*(double)x/1000.0))
#define MaxPWMCount 460
#define refTick 1.0/60.0/((float)MaxPWMCount)/(1.0/48.0e6)
#define MaxPWMCountdiv2 MaxPWMCount/2


/* Timer_A PWM Configuration Parameter */
Timer_A_PWMConfig pwmConfig =
{
TIMER_A_CLOCKSOURCE_SMCLK,
TIMER_A_CLOCKSOURCE_DIVIDER_1,
MaxPWMCount,
TIMER_A_CAPTURECOMPARE_REGISTER_1,
TIMER_A_OUTPUTMODE_RESET_SET,
32
};

unsigned short sinTable[MaxPWMCount];
int sysTickCounter;
int sinIndex;
int loopCount;


float reference;

int main(void)

{
volatile unsigned int i;

MAP_WDT_A_holdTimer();
MAP_FPU_enableModule();
MAP_FPU_enableLazyStacking();

int i2;

//Set up the table of sin values to be used as a reference to the control system.
for(i2=0;i2<MaxPWMCount;i2++)
{

//sinTable[i2] = 800.0f/2.0f*(sin(((float)i2)/((float)MaxPWMCount)*2.0f*3.14159265f));
sinTable[i2] = (((float)MaxPWMCount)-20.0f)/2.0f*(sin(((float)i2)/((float)MaxPWMCount)*2.0f*3.14159265f)+1.0f)+10.0f;
}


/* Set the core voltage level to VCORE1 for max clock speed and performance */
MAP_PCM_setCoreVoltageLevel(PCM_VCORE1);

/* Set 2 flash wait states for Flash bank 0 and 1*/
MAP_FlashCtl_setWaitState(FLASH_BANK0, 2);
MAP_FlashCtl_setWaitState(FLASH_BANK1, 2);

/* Initialize Clock System */
//Digitally Controlled Oscillator set to 48MHz
MAP_CS_setDCOCenteredFrequency(CS_DCO_FREQUENCY_48);
MAP_CS_initClockSignal(CS_MCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1 );
MAP_CS_initClockSignal(CS_HSMCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1 );
MAP_CS_initClockSignal(CS_SMCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1 );
MAP_CS_initClockSignal(CS_ACLK, CS_REFOCLK_SELECT, CS_CLOCK_DIVIDER_1);

//-------------------------------------------------------------------------


/* Configuring GPIO2.4 as peripheral output for PWM and NOT P6.7 for button
* interrupt but pin 5 for debug output*/
MAP_GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P2, GPIO_PIN4,
GPIO_PRIMARY_MODULE_FUNCTION);

MAP_GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN5);

/* Configuring Timer_A */
MAP_Timer_A_generatePWM(TIMER_A0_BASE, &pwmConfig);


/* Enabling interrupts and starting the watchdog timer */\

MAP_Interrupt_enableMaster();


//*****************************SYSTICK SETUP********************************************

/* Configuring SysTick to trigger at 100kHz (48MHz clock freq) */
MAP_SysTick_enableModule();

MAP_SysTick_setPeriod((int)refTick*5);

MAP_SysTick_enableInterrupt();

P5->SEL0 |= BIT4;
P5->SEL1 |= BIT5;
P5->SEL0 |= BIT5;
P5->DIR &= ~BIT5;
P5->DIR &= ~BIT4;


// Enable global interrupt
__enable_irq();

while (1)
{
__no_operation();
}
}


void SysTick_Handler(void)
{
int loop;

sinIndex++;
if(sinIndex==MaxPWMCount) sinIndex = 0;
reference = sinTable[sinIndex];
TIMER_A0->CCR[1] = reference;
MAP_GPIO_toggleOutputOnPin(GPIO_PORT_P1, GPIO_PIN5);
}

**Attention** This is a public forum