Part Number: MSP430FR2355
Other Parts Discussed in Thread: MSP430FR2353
Hello all,
I'am trying to implement a pulse oximeter design using MSP430FR2355 Launchpad. I've been following the reference design document SLAA274 & SLAA458. I came across one more TI Document SLAA897 in which the design is much efficient and required few external components.. As per the design of SLAA897 shown below
The Nellcor Compatible SPO2 Probe Pin diagram , PIN 2 is IRLED, PIN 3 IS RED LED, PIN 6 & 7 ARE GND.
Pin 9 is the output of photodiode cathode, & Pin 5 is the transimpedance offset pin.
Where to connect the Pin 5 As per the design in SLAA897?
Also should I connect the OA0 output to the OA2 inverting input externally or there is a way to connect it internally through Software?
Also is there any schematic and reference code of the design shown in document SLAA897?