This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi all,
I am having MSP430G2 Launchpad and DRV8711 boost pack to run the stepper motor.
I am using CCS10.0.0.00010
I downloaded the reference files (application and GUI) from the website
https://www.ti.com/tool/BOOST-DRV8711
As mentioned in the DRV8711 user guide, I used method 2 for importing the ccs project and downloaded to MSP430 Launchpad. This is fine no issue noticed during application loading.
Now I want to open the GUI composer, where it is?
In CCS, view->GUI composer->Designer (Online) is only available. In that if I select the "import existing project and select BOOST-DRV8711_GUIv1.0.exe" it shows as
"FAILED TO EXTRACT PROJECT FILES. REASON: ERROR: INVALID SIGNATURE 0x905a4d"
Can anyone suggest how to run the stepper motor in following two conditions:
1) MSP430 Launchpad + DRV8711 boos pack with GUI (ie GUI for setting the parameters and start stop command)
2) MSP430 Launchpad + DRV8711 boos pack without GUI (ie In MSP code itself for setting the parameters and GPIO to start/STOP)
Thanks and Regards,
Iyyappan.V
Iyyappan_krish@yahoo.co.in
Hi Iyyappan,
I think this document should helpful for you:
https://www.ti.com/lit/ug/slvu967a/slvu967a.pdf
And looks like there are some error about screenshot your upload , could you upload again?
Best Regards
Johnson
**Attention** This is a public forum