Part Number: MSP-FET
Other Parts Discussed in Thread: MSP430F5522, UNIFLASH
Tool/software: Code Composer Studio
Hello,
I haven't used my black MSP-FET in a while. Yesterday I plugged it into my Windows 10 PC and launched CCS10, and was told the programmer needed a firmware update. At first, the update has failed, leading me to ditch the USB hub that the device was originally connected through. The second time it seemed to have gone fine, after a minute or two, I was brought back to the main screen without any confirmation of update success.
After the update, my device has started acting weird. Upon connecting the device, the green "Power" LED turns ON, and the device is unresponsive. After exactly 30 seconds, the green LED turns OFF, the red "Mode" light turns ON. When I try to debug my target board (a custom board with a MSP430F5522), the CSS throws an error "unknown device". I confirm the board is good because I was able to successfully debug the board using another FET device I normally use.
Upon reading the user guide for FET, the "red LED ON, green LED OFF" scenario often occurs when the target Vcc is erroneous, or the USB cable is defective. My situation is strange because I get to this state without having the FET connected to target devices. I made sure my USB cable was good by connecting to and using the other FET device I normally use.
In order to identify the issue, I used MSP Flasher V1.3.20. It seems like the PC recognized the FET device, is able to confirm the firmware is up-to-date while the FET is in "error" state, but is either not able to provide Vcc to the target (error 44), or is not able to recognize the device (error 16).
Any suggestions on how to fix the FET device, or how can I further isolate the issue, is greatly appreciated.
Thank you!
Wenbo