I have just got the MSP-FET and tried to connect it to the MSP432P401R Launchpad.
I disconnected the jumpers of the TMS TCK TDI TDO from the LAUNCHPAD and connected the TCK and TMS from the MSP-FET to the TCK and TMS of the MSP432P402 side of the jumpers.
First I tried to connect the MSP-FET, I didn't see any MSP-FET option on the Connection option in project properties.
I selected the TI MSP430 USB1 option, the IDE started to update firmware and the system went into endless tries to update the firmware.
Now when I connect the USB cable to the MSP, i don't see any new devices in the PC Device manager under USB controllers.
is there a way to recover? how do i connect the MSP-FET to my target, do I need any intermediate board or can i just connect the GND and the TMS, TCK signal (this is what i did when i debugged my target using the LAUNCHPED XDS debbuger)
please advise,
shai.