Other Parts Discussed in Thread: TMP117EVM, , MSP-FET430UIF, USB2ANY
Hello,
tried to flash an MSP430F5528 located on a TMP117EVM with the help of MSP-FET430UIF. (SPI-Bi wire)
Do have two TMP117EVMs. On flashs without problem the other one shows mentioned error message.
With exactly the same command line!
The one showing the mentioned error can be flashed with IAR without any problem!
As I cannot use IAR to flash a .txt file without having the source code -> cannot flash the TMP117EVB with its original firmware.
Do not have other flash program than this.
This was the command line:
MSP430Flasher -n MSP430F5528 -w 4130.USB2ANY_F5528.txt -v -z [VCC] (-i USB) (-e ERASE_ALL)
C:\EE\ti\MSPFlasher_1.3.20> MSP430Flasher -n MSP430F5528 -w 4130.USB2ANY_F5528.txt -v -z [VCC] (-i USB) (-e ERASE_ALL)
* -----/|-------------------------------------------------------------------- *
* / |__ *
* /_ / MSP Flasher v1.3.20 *
* | / *
* -----|/-------------------------------------------------------------------- *
*
* Evaluating triggers...done
* Checking for available FET debuggers:
* Found USB FET @ COM10 <- Selected
* Initializing interface @ COM10...done
* Checking firmware compatibility:
* FET firmware is up to date.
* Reading FW version...done
* Setting VCC to 3000 mV...done
* Accessing device...
# Exit: 16
# ERROR: Unknown device
* Starting target code execution...done
* Disconnecting from device...done
*
* ----------------------------------------------------------------------------
* Driver : closed (Internal error)
* ----------------------------------------------------------------------------
*/
Thanks& Regards
Michael