This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
trying to get a the DRV8711 + MSP430-EXP430G2ET running first time.
Motor and power supply connected
set up the Hardware/Software as advised in User's Guide SLVU967–May 2014.
The Gui is running and seems connected with the DRV8711 Controller. But the Software Buttons are not working .
Another indication for dysfunction is the emty Firmware Version window and and full scale current widow.
Can you help me to get it run , any clue ?
unfortunattelly not. Is there anything i can check ?
i can imagine that an unequal baudrate setting launchpad <> DRV8711 can causes a miscommunication, would you agree ? if yes how can i set baudrate of DRV8711 ?
thanks
Hey Matthias,
Unfortunately, I was unable to get this GUI to run on my machine to try and debug on my side. I'm going to reach out to the DRV team as one of them should have it running.
In the mean time, Can you please confirm these things from your side:
1. Have You successfully programmed the BOOST-DRV8711_FIRMWARE into the MSP430 Launchpad?
2. Can you confirm the jumper settings match the DRV8711 EVM User's guide?
Thanks,
JD
yes , i did all of this. my board is an MSP430G2ET.
serial monitor shows no interaction with the board until i deactivated the fifo button in windows com config.
No the Gui works but extremly slow.
**Attention** This is a public forum