This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353R:GDUV error active when using DRV8353RS

Part Number: DRV8353R
Other Parts Discussed in Thread: CSD19532Q5B, DRV8353

Tool/software:

This is a continuation of the previous question.
I checked the datasheet of DRV8353RS and it says that GDUV should be 0 at Addr 1 for SPI communication.
However, in the same datasheet, it says something like the picture below.
Which is correct, 0 or 1? I ask because sometimes there are typos in the SPI communication data as well.

On power-up, the GDUV is enabled as shown below.
Replacing the DRV8353RS and the MOSFET causes the same symptoms.
In your previous question, you suggested using CLR_FLT to perform an initialisation, I tried it but the same result occurs.

The MOSFET is using CSD19532Q5B. Have a nice day and look forward to your reply.