This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO5852S-Q1: DESAT protection

Part Number: ISO5852S-Q1

Hi,

We are designing gate driver for IGBT(IKW40N120CS6) which short circuit handling time is very low (3us), for such short time DESAT protection if we calculate blanking capacitor using current source of 0.5mA, it will come around 15pF. If we are placing such small capacitor DESAT protection getting triggered frequently, I think it is due to charging current during turn-off through blocking diode parasitic capacitor. 

1. Am I thinking in right direction?

2. Is there any way we can increase detection time without reducing blanking capacitor?