Other Parts Discussed in Thread: PMP8803, TPS23756, TPS2376, TPS23756EVM
Hello Team,
We are using TPS23753A in our design ,
input requirement
1. from PSE 48V
2. 24V AC
3. 12V DC
output required
12V DC
The first input 48VAC will come from the PoE injector and we have RJ45 jack for that , the second input 24VAC will have connector on the board and for the 12V DC we are using same connector as used for 24VAC.
That means from one connector both 24VAC and 12V DC will be injected .such kind of configuration are used in the IP Camera .
SLUA477 application note provide the design for the 48VAC and 24VAC to 12V DC , But by concern is how can i provide 12V DC input to the 24VAC connector ,how can i bypass or switch between the 24VAC and 12V DC input . I have done some research and found that we can use relay for this purpose , but i am not sure how the circuit will work .
I have one reference schematic with me
Please help to explain the this 24VAC and 12VDC input section working , also if TI has some similar supported solution please provide that too