Other Parts Discussed in Thread: LM27761, LM339A
According to the data sheet, the formula for Vout is -1.22*(R1+R2)/R2
where Vfb should be (1.22) between 1.202V and 1.238V
So I choose R1=115K and R2=499K to get Vout=-1.5V
However Vout turns out to be either -1.5V(with Vfb=-1.219) or -2.31V (with Vfb=-1.877)
I verified that Vfb is connected to the voltage divider.
What am I doing wrong?
What in the chip should be forcing Vfb to go to -1.22 instead of -1.877?
Thank you in advance for your assistance.