Other Parts Discussed in Thread: BQ76952
Hello,
I have a problem with my 8 cell battery monitor circuit which was worked perfectly till some point.
Schematic is here:8cellBQ76942monitor.pdf
In compare to default settings I wrote to OTP some changes, but after that everything was working fine for more than 2 weeks, so I'm sure that this is not source of the problem. However, here is the list of settings I wrote to OTP::
REG12 Config :: 00 (default) -> 0D (new value)
REG0 Config :: 00 (default) -> 01 (new value)
I2C Address :: 00 (default) -> 60 (new value)
Alert Pin Config :: 00 (default) -> 29 (new value)
TS1 Config :: 07 (default) -> 0B (new value)
The problem is that device is not detected on I2C bus. Additionally there is no 3.3 V on the regulator's (REG1) output and I can measure that on REG18 pin is only 0.975 V instead of 1.8 V. I also tried to wake-up an IC with switch on TS2 but It doesn't help.
What are possible reasons for this issue?
Many thanks,
Kind regards,
Dejan.