This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610: How to disable temperature check ?

Part Number: BQ24610

Since, cut off high temperature is 34% of Vref and cold temperature cut off is 74% of Vref, can we use a voltage divider from Vref with 2 resistors as 5.1kOhm to disable the temperature sensing as it will be at 50% of Vref always ? Or are there any other methods of disabling temperature qualification checks ?

Thanks in advance