This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
First decide at which current you want to trigger CS1 and which current you want to trigger CS2. Then divide that current by 100, then times the current after division with a resistor value to get the CS1 and CS2 threshold.
Hi,
May I ask which resistor you were referring to when you multiplied the resistor value earlier?
Hi,
R3 and R4 for the EVM for CS1. CS2 has divider of R6 and R7. You need to converter 33A to the primary side first then do the calculation of CS1 and CS2.
You can use the below LM5025A design calculator for your design.
Sorry, the CS2 voltage I calculated is still very incorrect. Could you tell me where I made a mistake? When the secondary side is at 33A, the primary side is 3.03A.
(3.03A/100)*R2*(R7/R6+R7)=39.6V
Hi,
R3//R4 does show in your calculation, why R2.
33A is average you need to use peak current.
But the big error should be R3//R4 not in your calculation.
Hi,
Is this the correct calculation method?
(4.28A/100)*(R2//R3//R4//(R6+R7))*(R6/R6+R7)=0.046V
Hi,
The resistor values are from the bench tune up due to leakage spikes and capacitor charges. Also at high line of input voltage to deliver same average 33A current peak current will be much higher than low line due to different duty cycle. So these will make difference between calculation and bench reality. The calculation process is correct. You can follow that but you will need to tune up.
Hi,
It is to help reduce power losses compared to use a resistor for current sense.