This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
Our schematic as below, if V_ADP Floating plug in battery Pack, then VBAT1=12V U2's VSW=29~32V, U2 or U1 damage.
The Battery Pack is 3 cell 12.x voltage. why this schematic have boost from VBAT1?
Please use fresh units and show scope capture at the battery insertion. Probe at VBAT1, VSW .
When adapter is not present, plugging in VBAT should bq24610 should not switch. Therefore, it is very unlikely to have 29V at SW node with 12V battery hotplug in.
Hi Sir,
We are remove the Q40's R736 & C579, the VSW never boost to 28~32V to damage BQ24610 & CSD87330.
Why this boost is Through R736 & C579?
As I know, TI BQ24610EVM is suggest the Q1 & Q2 on input side.
if we want to cost down one MOSFET, How to design? similar BQ24170 datasheet page 28 Q4 is OK?
Ch3= U2 Pin3
Ch4= U2 Pin5
Hi Sir,
We are try to remove BQ24610EVM Q5, but we are see the VSW have boost 18V voltage & current probe measure 66,4A.
if we add Q5 same condition on customer PCB, then boost issue solve Rise is Smooth.
if this application only 5~6 charger docking board not have system side on PCB, then Q5 is must? or change to Schottky or diode? or any suggest share for me?
The first peak current is to charge up the cap on the board. The second peak is what we should look at.
Without Q5 current directly goes through inductor to charge the input caps thus you will see the VSW overshoot.
If there is no system, you can use shottcky diode instead.