This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have started to use BQ24610 in order to charge a Li-ION battery of 2x5 cells, up to 21V.
The essence of the problem in the following:
Our system is externally powered, we only use the BQ24610 to charge the battery, and we have found that when we connect the battery when the system is unpowered, somehow the BQ24610 burns, because it stops responding (for example, we don't observe 3V3 in the VREF pin). It seems that there is a reverse current from the battery to the system. When we use another board, first powering the board and after connecting the battery, it works perfectly fine. This "burn effect" has happened in three circuit boards.Sheet1.SchDoc
Hi,
There is a path to SYSTEM through the body diode of the HSFET. Do you have any SYSTEM load? Your input trace is labeled VBAT. What VBAT is the source for the charger IC?
VBAT is the input supply voltage of the board, and of the BQ24610, it's 24V. And we don't have any SYSTEM load.
What are you using for your source? Is it a lead acid battery? As BATDRV is not connected it does not look like you are using the powerpath feature. Can you describe the connection of your externally powered system?