This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6548: Linux reboot command fails

Part Number: AM6548

As of SDK 7.3, Linux reboot command fails on AM654, because of a board issue while switching voltages for MMC UHS modes. A workaround is to disable UHS modes and remove the vmmc supply control to MMC controller. This can be done by making the following changes in the sdhci1 device tree node.

  1. add no-1-8-v tag
  2. remove the "vmmc-supply" property

Please refer to the attachment for a patch that applies the above workaround.

Currently, UHS modes are only supported on AM65 P.G. 2.0 and by applying this workaround this will be disabled.

https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/0001_2D00_HACK_2D00_arm64_2D00_dts_2D00_k3_2D00_am654_2D00_base_2D00_board_2D00_Workaround_2D00_to_2D00_add.patch